This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Dual LAN device

Dear Community,

I am looking for a device which has dual LAN interfaces. Each of which are connected to a separate network with different network settings. Both interfaces should be configured differently. Can you recommend any device from TI?

I would like to run some basic network services like: DHCP server, FTP server, SNMP, etc...on the LAN1 however on the LAN2 I need only static IP configuration and an FTP server. Do you think that an SPI-based Ethernet can help me? I am using TI-RTOS on TM4C. Is there any booster pack for that? 

Looking forward you kind reply!