Part Number: AM5728
Tool/software: TI-RTOS
HI everybody ,
I am on IDK , I am using Uart everything is fine @ 115200 baud . now I need 921600 , I set as code hereunder but both TX and RX speed are wrong ( it seems to be 996720[bps]. )
where am I wrong ?
here is the code
uartParams.parityType = uartParity;
// *** At this place we can also change baud-rate settings etc.!!! ***
uartParams.baudRate = 921600; // Change the baud-rate from default 115200 to something else
// *************************************************************************
// Open a UART instance with the given UART parameters and receive a handle.
// *************************************************************************
uart = UART_open(uartTestInstance, &uartParams);
if (uart == NULL)
thank you very much
regards
Carlo