I've a 128MB DDR, and my bootargs is "mem=60m"
When the Linux booted, the system use about 20M
When I load dsp.out, the load program use about 11M
And my arm-side program use about 35M, when I run it, then error occrus:
"Segment fault" or "Can't load shared lib xxx.so",
So I try to set the bootargs to "mem=100m", and modify the dsp project file dsplink-omapl138gem-base.tci
"RESET_VECTOR.base" from 0xc3e00000 ( 62M ) to 0xc64000000(100M)
But this time, I've got the error "memory size is wrong" when I load dsp.out
I think I've to also modify some code to rebuild dsplinkk.ko, right?
So what should I do and how to rebuild ko file, just like rebuild all " make dsplink _clean ; make dsplink"
or just get into some folder and only rebuild dsplinkk.ko?
Another question, when I modified the kernel src, do I need the rebuild the ko file, I think ko file is a driver and it need to be rebuilded,
but I found it doesn't need?
Last question, can dsp.out run on it's inner-Ram, not DDR?