Hello.
I'm developing a camera application using TDA2Px EVM and Fusion Application Board.
Fusion application board has two UB960 deserializers, and an issue has arisen that requires changing the register value of UB960 to use the new camera.
However, it is difficult to find a user guide or datasheet of UB960.
Where can I get a user guide or datasheet of UB960?
One more thing, I wonder if there are four i2c addresses that need to be changed for communication with the new Camera. : Serializer's real address(0x5D)and alias address(0x60), Sensor's real address(0x5E)and alias address(0x66).
Thank you.