Other Parts Discussed in Thread: TMS320C6424
Hello
I have a board with TMS320c6424 configured to use UART0 HW flow control Boot mode, Little Endian, Slow Boot.
When the DSP is powered up I get on the UART0 BOOT ERR instead of BOOT ME.
If I upload an AIS file the DSP respond with DONE, and the application is not executed. Then I upload again the AIS file, at the end again I get the DONE message but this time the application is executed.
If I read the BOOTCFG ( 0x01C4 0014 ) register then I get the value 0x10000E. This mean that I have Little endian and UART0 HW flow control,slow boot.
So where is the problem?
Br
Robert.