Other Parts Discussed in Thread: OMAP-L138, AM1808
Stated in every Terminal Function table in the OMAP-L138/AM1808 datasheets:
IPD = Internal Pulldown resistor; IPU = Internal Pullup resistor; CP[n] = configurable pull-up/pull-down (where n is the pin group) using
the PUPDENA and PUPDSEL registers in the System Module. The pull-up and pull-down control of these pins is not active until the
device is out of reset. During reset, all of the pins associated with these registers are weakly pulled down. If the application requires a
pull-up, an external pull-up can be used.
How soon after reset is de-asserted do the internal pullup/pulldown resistor become active? Do the pins go back to being weakly pulled down during a Warm Reset?