Hello DSP experts,
I'm new to the DSP world, so please forgive any childish questions I might have.
I have a requirement from my customer to pass 24 bit color depth - RGB888 to a serializer (LVDS type) and I was planning of using TMS320DM6437ZWTO5. It seems like the VPBE of this DSP can handle that, but I'm not sure on the VPFE side, the CCD Controller can handle RGB888 from the image sensor. I realize the VPFE could handle RGB656 or YCbCr 422, and VPBE could convert it to RGB888, but wouldn't some color information be lost in such a conversion?
The image sensor is not under my control and I don't know its specs yet. I have to assume it's 768 X 506 and 30 fps, and works at 95 MHz PCLK.
My question is - can TMS320DM6437ZWTQ5's CCDC handle RGB888, or should I go to a higher frequency DSP (TMS320DM6437ZWTQ6), or a different DSP family alltogether?
Thank you,
ChrisM