This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

H.264 Baseline Profile Decoder on C64x+

Hi all,

   I have few queries w.r.t the SPRS315c(H.264 Baseline Profile Decoder
(2.00) on C64x+) datasheet, in which Table 2 includes Cycle information
- profiled on dm644x EVM With Code Generation Tools Version 6.0.8.

i would like to know

1) whether the average and peak MCPS mentioned for the various testvectors
includes Deblocking filter module or not?

2) why there isnt any linear proportionality in terms of avg and peak MCPS between the following vectors(QCIF and D1) ?  

 i )FM1_BT_B.264,YUV422ILE, FMO with all types of slice-groups, QCIF(176x144),
270@ kbps ->  60(avg MCPS) and 88(peak MCPS)

 ii)fire_30frames_2_Mbps.264, YUV422ILE, 16MV, D1(720x480), @ 2 mbps -> 292(avgMCPS)  and 311(peak MCPS)

3) If deblocking filter cycle count is included in the MCPS results.what percentage do they
contribute in a QCIF and D1 vector?

Eagerly waiting for ur replies/suggestions.

Regards,
Sandeep