Tool/software: Linux
Is Vision SDK not supported in Linux Host Machine to be used for TDA3x EVM or TDA3x RVP?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Linux
Is Vision SDK not supported in Linux Host Machine to be used for TDA3x EVM or TDA3x RVP?
Yes, it is supported on Linux. But in the UserGuide it is mentioned that the SDK only supports TDA2x, TDA2PX etc.. but it doesn't mention about TDA3x. Can you please confirm if SDK on Linux supports TDA3x ?
Hi Rishabh,
I downloaded the linux installer from here: http://software-dl.ti.com/processor-sdk-vision/esd/TDAx/vision-sdk/latest/index_FDS.html
In the Docs, there is "VisionSDK_Linux_UserGuide". Go to page 5, section 2.3. It mentions that this SDK release supports only TDA2x, TDA2EX and TDA2PX EVMs. I have a TDA3x Starter Kit and TDA3x RVP from D3 Engineering. I want to know if this SDK can be used for the hardware I have.
If not, Is using Windows SDK the only option for me? I prefer using Linux installer as we use Ubuntu as our main development environment and would like to know any other options we have.
Thanks,
Keerthi
Rishabh,
I want to install the Vision SDK on a Linux Ubuntu 14.04 computer. I know that TDA3x itself cannot host linux on it, so BIOS will be used.