This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

vlynq support

Hi,

I'm trying to interface to an altera fgpa throuh vlynq with DM6467 as master and TES altera VLYNQ IP.

When I insmod saVlynq.ko, I get

Starting Vlynq Test Case...

VLYNQ MASTER:Success in Initializing vlynq configuration

VLYNQ ID from config_bridge = 0

Link not detected 1

VLYNQ MASTER: Failed to initialize the vlynq 0xc8430000

VLYNQ MASTER:The error msg: Error in configuring clocks.

VLYNQ MASTER:Error in LOCAL & PEER vlynq configuration.

VLYNQ Initialization Failed.

 

when the FPGA IP is not correctly connected. 

 

Otherwise, my kernel hangs with no error message.  In that case, Bit 0 in the VLYNQ status register (LINK bit) is set to 1.

 

What can cause the system to hang when I try to initialize the link with the FPGA.

 

Thanks

Yann