This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3358: ePWM synchronization

Part Number: AM3358

Hello 

I pretend to work with the input synchronization of ePWM with AM3358, from external hardware (GPS at 1pps) which is a synchronized event. 

Looking in datasheet, figure below, I see that if I enable TBCTL[CNTLDE], which is wrong in datasheet it was supposed to be  TBCTL[PHSEN], is enough to work when a event occur in EPWMxSYNCIN. 

So my question is when the synchronization event occur the counter is reset or only loaded to the TBPHS value?

Which suggestions would you give me? This is best solution for my case or do you think is best to work with interruptions??

Thanks in advance