This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Quick question about CCS: how to work with 2 targets without adding/deleting the connection every time



Hello,

        we have two different evaluation boards in our lab. In one we use the Jtag-cable and in the other usb connection(dm6437). Every time that I click on the CCS shortcut dm6437, it seems that automatically remove the J-tag connection, because later to connect the other we need to enter again in the setup of CCS to add the jtag connection of the other board, and is very annoying. Does anyone knows if it is possible to configure CCS to work with both boards without configuring the connection everytime?

 

thank you