This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/DRA746: Weston/wayland debugging .

Part Number: DRA746

Tool/software: Linux

Hello Team, 

We use custom h/w and software based on DRA746 and SDK 3.02.00.03 with wayland 1.11.We have two quires here: 

1. Weston crash dump analysis:

            During our testing some times we got weston crash issue and some of these weston crash issue are of once occurrence.

            But we are not able to analyze the weston crash dump, we always get the corrupted backtrace with 1 or no trace. 

            Could you please help us in generating the backtrace of the weston crash.

2. For enabling the logging for weston.

             Is there a way by which we can enable the logging for weston and wayland-ivi-shell. With "export WAYLAND_DEBUG=1" we are not getting any logs for the applications runs from the HMI.

             Also is there a way by which we can get ilm calls trace, if we run any application?

Thanks and Regards,

Ikshwaku