Hello I am working with the PWM and trying to create exact pwm frequency of 1920Hz. I am working with epwm (not EHRPWM yet) time-based because of the
SYSCLKOUT = 100MHz I can't the exact PWM frequency of 1920Hz, using the formula below in up-mode.
What can I do to solve my problem?
Working with EHRPWM would be better? The frequency will be 1920Hz?
Another solution is to change the SYSCLKOUT for a multiple of 3 like 90MHz, is this effective?