Hi all,
I am new to Da-vinci.
I am developing a board using DM6467 and aiming to port Linux using NFS on the same. I have seen some baords like EVM6467 which are having Linux Booting Facility though NFS.
While implemeting this I have some basic doubts.
1. When I say DM6467 will boot in Linux via NFS there has to be a boot loader which is basically a EtherNet Controller (similar to when boot through Flash- Bootloader has read controller). If I refer to datasheet of DM6467 I can not find some booting mode which refers to this booting mode.
While if I refer EVM6467 it says there is EMAC boot mode (which I guess is NFS-boot mode)
In this case, do I have to write bootloader to for this application OR is it something that is some feature of DM6467 and I need not worry about ?
If I need to develop bootloader for NFS, is some reference code is available ?
Regards,
Onkar Patki