This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/AM5726: SDK installation issue

Part Number: AM5726

Tool/software: TI-RTOS

Hi everybody , 

please  I woudl like to have  on my PC multiple SDK  installation for history etc .  

Now  in installation I am following instruction to use a differnet PATH ( differnet from c:\ti  ) so to have  newer  PDK in  related dir .

what happened  to me was not able to run  gmake with error , it was missinig file  (  ti.utils.profiling.aa15fg    in 

C:\ti\pdk_am57xx_1_0_10\packages\ti\utils\profiling\lib\a15\release  ) .  I checked and the file was not there  , while on PC  where I did a Vanilla installation in C:\ti  the file was there .  druing SDK installation I did not get any error message 

question : why this file was not there ?     coudl be a issue on PATH  in term of lenght name for directory usage ?

coudl you kindly confirm   SDK installtion guideline in a differnet dir form C:\ti ?

thank you very much 

regards

Carlo

  • The RTOS team have been notified. They will respond here.
  • Carlo,

    The installer works the same way whether you install in C:\ti or in custom path.  Please refer to the screenshot below, I have installed the library in the path C:\ti\AM57x_PRSDK43 and you can see that the library is present.

    The only way this error can occur is when you accidentally remove the pre-built library using gmake clean or if the installation didn`t run to completion correctly. We have been installing Processor SDK RTOS in custom locations for the past two years and have run into no issues

    Regards,

    Rahul