Other Parts Discussed in Thread: TDA2
Hi,
We have TDA3x Starter Kit from D3. In the "VisionSDK_UserGuide_NetworkTools.pdf", there is following snippet:
When sending RAW/YUV frames
When NDK runs on M4 CPU, one can achieve a data rate of about 2 MB/s (16Mbps)
When NDK runs on A15 CPU (TDA2x or TDA2px), one can achieve a data rate of
about 60 MB/s (480Mbps)
Is the slow data rate of 2 MB/s because of the Ethernet PHY? or the M4 running at just ~200 Mhz? or is this only when using the network tool provided with the SDK?
Can we expect to send a 1080x720 YUV video at 20 fps over ethernet to a client machine (not using network tool)? We were under the asssumption that TDA3x has a Gigabit ethernet and this should be possible.
If this is not possible, what is the highest bandwidth we can achieve over ethernet among all the TDA family of processors? It seems like A15 on TDA2x can achieve up to 60 MB/s. May I know why this is significantly (30x) higher than TDA3x? Can we achieve more with any other device?
Thanks,
Keerthi