Tool/software: Linux
Hello, TI.
I am using am5728 to do some image processing work and I met some problems.
I want to read images from two cameras and do some work related to real-time stereo vision. While in practice, the delay between my action in reality and in screen is large,about 1s.
I have tried Videocapture::grab() but it doesn't work. The format coming from the two cameras is MJPEG.
I want to know if I can use the IPU(image processing unit) or DSP in target board to accelerate the decoding of the image.
Thanks.
Li Qi