This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVMK2H: Building the PDK

Part Number: EVMK2H
Other Parts Discussed in Thread: MATHLIB, TCI6638K2K

I tried to create the examples using the scripts provided in the PDK.

First i ran the setupenv script then the

creatproject, script the example projects will not build

the program discovers the projects but does not create them.

for each example project that it tried to create it returns

"The System cannot find the specified file"

I followed the steps from the webpage that shows you how to do this but i haven't been successful

  • Hi Alfredo,

    Could you post a link to the tutorial which you are follow?

    BR
    Tsvetolin Shulev
  • Here's what i followed

    processors.wiki.ti.com/.../Rebuilding_The_PDK

    Is there an order that the scripts have to be in, also i looked at the scripts and the PDK shortname appears wrong when the scripts' echo command displays the variable

    is there another tool that i am missing?

  • Try below steps,

    1. Open CCS and discover all the products that have been installed during the SDK installation.
    2. Have you installed processor SDK in default installation path ? If no then, please set the SDK_INSTALL_PATH to the correct path.
    3. Set TOOLS_INSTALL_PATH to point to directory where CCS is installed.
    4. Run the setupenv script.
    5. Run the pdk example script.
  • Alfredo,

    I ran into a similar problem once, and I seem to remember it being related to the system environment. There are a number of environment variables used in the pdkProjectCreate.sh script. I would recommend that you make sure CCS_INSTALL_PATH and TOOLS_INSTALL_PATH are set properly. If you have your SDK installed anywhere other than the default directory, the path will not be set correctly.

    Hope this helps,

    Jeff
  • CCS has already discovered it. Everything is in the default directory from install, Where do I set the path, is it in the script? Or while the script is running
  • You can set the environment variables in the shell (assuming Linux). You could also dig through the script and set them manually. It may help to look at how those variables are used in the script. Apart from that, I'll have to let the guys from TI help you out.
  • Not on script, set as environment variables. Please post the command used to create PDK examples here.

    Thank you.
  • Note: using Windows host

    Command used:
    pdkProjectCreate.bat K2H
  • I am unable to re-produce the issue here.

    1. What is the Processor SDK version used?
    2. In windows command prompt that is used to create exmaple, type the command "set" and attach the dump here.

    Thank you.
  • PDK used:
    pdk_k2hk_4_0_9

    Command entered:
    pdksetupenv.bat set

    output:
    Environment Configuration
    LIMIT_SOCS : k2h k2k
    LIMIT_BOARDS : evmK2H evmK2K
    PDK_INSTALL_PATH : /ti/PDK_K~2/packages/set
    IMG_LIB_INSTALL_PATH :c:/ti/imglib_c66x_3_1_1_0
    DSP_LIB_INSTALL_PATH :c:/ti/dpslib_c66x_3_4_0_0
    MATH_INSTALL_PATH :c:/ti/mathlib_c66x_3_1_1_0
    XDC_INSTALL_PATH ::c:/ti/xdctools_3_50_03_33_core
  • If I enter the command

    pdkProjectCreate.bat set

    what follows is:

    SOC ( set ) is invalid
  • Just type"set" on command prompt,

    C:\Users\Raj>
    C:\Users\Raj>set
    ALLUSERSPROFILE=C:\ProgramData
    APPDATA=C:\Users\x0189341\AppData\Roaming
    CommonProgramFiles=C:\Program Files\Common Files
    CommonProgramFiles(x86)=C:\Program Files (x86)\Common Files
    CommonProgramW6432=C:\Program Files\Common Files
    COMPUTERNAME=LTX0189341A
    ComSpec=C:\WINDOWS\system32\cmd.exe
    DADIR=C:\Program Files (x86)\CheckPoint\Endpoint Security\Endpoint Common
    DEVMGR_SHOW_DETAILS=1
    DEVMGR_SHOW_NONPRESENT_DEVICES=1
    ESDSERVER=dleesd.itg.ti.com
    HOMEDRIVE=C:
    HOMEPATH=\Users\x0189341
    IA_SDK_HOME=C:\ti\sysbios_ind_sdk_02.01.03.02\sdk
    LOCALAPPDATA=C:\Users\x0189341\AppData\Local
    LOGONSERVER=\\DFLAD03
    NUMBER_OF_PROCESSORS=4
    OneDrive=C:\Users\x0189341\OneDrive
    OS=Windows_NT
    Path=C:\Program Files (x86)\Common Files\Oracle\Java\javapath;C:\TwinCAT\Common64;C:\TwinCAT\Common32;C:\ProgramData\Oracle\Java\javapath;C:\WINDOWS\system32;C:\WINDOWS;C:\WINDOWS\System32\Wbem;C:\WINDOWS\System32\WindowsPowerShell\v1.0\;C:\Program Files (x86)\CheckPoint\Endpoint Security\Endpoint Common\bin;C:\Program Files (x86)\USB-IF Test Suite\USBET20\;C:\Program Files (x86)\Pico Technology\Pico Full\;C:\Program Files\PuTTY\;C:\Users\x0189341\AppData\Local\Microsoft\WindowsApps;
    PATHEXT=.COM;.EXE;.BAT;.CMD;.VBS;.VBE;.JS;.JSE;.WSF;.WSH;.MSC
    PROCESSOR_ARCHITECTURE=AMD64
    PROCESSOR_IDENTIFIER=Intel64 Family 6 Model 61 Stepping 4, GenuineIntel
    PROCESSOR_LEVEL=6
    PROCESSOR_REVISION=3d04
    ProgramData=C:\ProgramData
    ProgramFiles=C:\Program Files
    ProgramFiles(x86)=C:\Program Files (x86)
    ProgramW6432=C:\Program Files
    PROMPT=$P$G
    PSModulePath=C:\Program Files\WindowsPowerShell\Modules;C:\WINDOWS\system32\WindowsPowerShell\v1.0\Modules
    PUBLIC=C:\Users\Public
    SDK_INSTALL_PATH="c:\ti"
    SESSIONNAME=Console
    SystemDrive=C:
    SystemRoot=C:\WINDOWS
    TEMP=C:\Users\x0189341\AppData\Local\Temp
    TMP=C:\Users\x0189341\AppData\Local\Temp
    TOOLS_INSTALL_PATH="c:\ti"
    TWINCAT3DIR=C:\TwinCAT\3.1\
    TWINCATSDK=C:\TwinCAT\3.1\SDK\
    UATDATA=C:\WINDOWS\CCM\UATData\D9F8C395-CAB8-491d-B8AC-179A1FE1BE77
    USERDNSDOMAIN=ENT.TI.COM
    USERDOMAIN=ENT
    USERDOMAIN_ROAMINGPROFILE=ENT
    USERNAME=x0189341
    USERPROFILE=C:\Users\x0189341
    windir=C:\WINDOWS
    
    C:\Users\Raj>
    

  • Here's My Output

    C:\>set
    ALLUSERSPROFILE=C:\ProgramData
    APPDATA=C:\Users\Freddy\AppData\Roaming
    BRB=c:\Program Files\HP\Sure Click\bin
    BRS=c:\Program Files\HP\Sure Click\servers
    CommonProgramFiles=C:\Program Files\Common Files
    CommonProgramFiles(x86)=C:\Program Files (x86)\Common Files
    CommonProgramW6432=C:\Program Files\Common Files
    ComSpec=C:\windows\system32\cmd.exe
    DSPLIB_INSTALL_PATH=C:/ti/dsplib_c66x_3_4_0_0
    DSPLIB_VERSION=c66x_3_4_0_0
    HOMEDRIVE=C:
    IMGLIB_INSTALL_PATH=C:/ti/imglib_c66x_3_1_1_0
    IMGLIB_VERSION=c66x_3_1_1_0
    IPC_INSTALL_PATH=C:/ti/ipc_3_47_01_00
    IPC_VERSION=3_47_01_00
    LIMIT_BOARDS=evmK2H evmK2K
    LIMIT_SOCS=k2h k2k
    LOCALAPPDATA=C:\Users\Freddy\AppData\Local
    LOGONSERVER=\\DESKTOP-7KK6AQI
    MATHLIB_INSTALL_PATH=C:/ti/mathlib_c66x_3_1_1_0
    MATHLIB_VERSION=c66x_3_1_1_0
    NUMBER_OF_PROCESSORS=8
    OnlineServices=Online Services
    OS=Windows_NT
    Path=C:/Windows/System32;C:/ti/xdctools_3_50_03_33_core;C:/ti/xdctools_3_50_03_33_core\bin;C:/ti/xdctools_3_50_03_33_core\packages\xdc\services\io\release
    PATHEXT=.COM;.EXE;.BAT;.CMD;.VBS;.VBE;.JS;.JSE;.WSF;.WSH;.MSC
    PDK_INSTALL_PATH=/ti/PDK_K2~2/packages
    PDK_PATH=C:\ti\pdk_k2hk_4_0_9
    PDK_SHORT_NAME=C:\ti\pdk_k2hk_4_0_9\packages
    PDK_SOC=k2hk
    PDK_VERSION=4_0_9
    platformcode=7F
    PROCESSOR_ARCHITECTURE=AMD64
    PROCESSOR_IDENTIFIER=Intel64 Family 6 Model 158 Stepping 9, GenuineIntel
    PROCESSOR_LEVEL=6
    PROCESSOR_REVISION=9e09
    ProgramData=C:\ProgramData
    ProgramFiles=C:\Program Files
    ProgramFiles(x86)=C:\Program Files (x86)
    ProgramW6432=C:\Program Files
    PROMPT=$P$G
    PSModulePath=C:\Program Files\WindowsPowerShell\Modules;C:\windows\system32\WindowsPowerShell\v1.0\Modules;c:\Program Files\Intel\Wired Networking\
    PTSMINSTALLPATH=c:\Program Files\HP\HP ProtectTools Security Manager\Bin\
    PTSMINSTALLPATH_X86=c:\Program Files (x86)\HP\HP ProtectTools Security Manager\Bin\
    PUBLIC=C:\Users\Public
    RegionCode=NA
    SDK_INSTALL_PATH=C:/ti
    SESSIONNAME=Console
    SystemDrive=C:
    SystemRoot=C:\windows
    windir=C:\windows
    XDCROOT=C:\ti\xdctools_3_50_05_12_core
    XDC_INSTALL_PATH=C:/ti/xdctools_3_50_03_33_core
    XDC_VERSION=3_50_03_33_core

  • TOOLS_INSTALL_PATH is missing on your environment variable. Set the tools path and try building the pdk example.

    > set TOOLS_INSTALL_PATH="c:\ti"
  • I added the TOOLS_INSTALL_PATH as mentioned above
    ran the script twice with and without quotes but i still get the same results
    Here are my results:

    C:\ti\pdk_k2hk_4_0_9\packages>set
    ALLUSERSPROFILE=C:\ProgramData
    APPDATA=C:\Users\Freddy\AppData\Roaming
    BRB=c:\Program Files\HP\Sure Click\bin
    BRS=c:\Program Files\HP\Sure Click\servers
    CommonProgramFiles=C:\Program Files\Common Files
    CommonProgramFiles(x86)=C:\Program Files (x86)\Common Files
    CommonProgramW6432=C:\Program Files\Common Files
    COMPUTERNAME=DESKTOP-7KK6AQI
    ComSpec=C:\windows\system32\cmd.exe
    HOMEDRIVE=C:
    HOMEPATH=\Users\Freddy
    LOCALAPPDATA=C:\Users\Freddy\AppData\Local
    LOGONSERVER=\\DESKTOP-7KK6AQI
    NUMBER_OF_PROCESSORS=8
    OneDrive=C:\Users\Freddy\OneDrive
    OnlineServices=Online Services
    OS=Windows_NT
    Path=C:\ti\xdctools_3_50_05_12_core;C:\Program Files (x86)\Intel\iCLS Client\;C:\Program Files\Intel\iCLS Client\;C:\windows\system32;C:\windows;C:\windows\System32\Wbem;C:\windows\System32\WindowsPowerShell\v1.0\;C:\Program Files (x86)\Intel\Intel(R) Management Engine Components\DAL;C:\Program Files\Intel\Intel(R) Management Engine Components\DAL;C:\Program Files (x86)\Intel\Intel(R) Management Engine Components\IPT;C:\Program Files\Intel\Intel(R) Management Engine Components\IPT;C:\Program Files\Intel\WiFi\bin\;C:\Program Files\Common Files\Intel\WirelessCommon\;C:\Python27;C:\Program Files\doxygen\bin;PDK_INSTALL_PATH;C:\ti\xdctools_3_50_05_12_core;C:\Users\Freddy\AppData\Local\Microsoft\WindowsApps;
    PATHEXT=.COM;.EXE;.BAT;.CMD;.VBS;.VBE;.JS;.JSE;.WSF;.WSH;.MSC
    PDK_INSTALL_PATH=C:\ti\pdk_k2hk_4_0_9\packages
    PDK_PATH=C:\ti\pdk_k2hk_4_0_9
    PDK_SHORT_NAME=C:\ti\pdk_k2hk_4_0_9\packages
    platformcode=7F
    PROCESSOR_ARCHITECTURE=AMD64
    PROCESSOR_IDENTIFIER=Intel64 Family 6 Model 158 Stepping 9, GenuineIntel
    PROCESSOR_LEVEL=6
    PROCESSOR_REVISION=9e09
    ProgramData=C:\ProgramData
    ProgramFiles=C:\Program Files
    ProgramFiles(x86)=C:\Program Files (x86)
    ProgramW6432=C:\Program Files
    PROMPT=$P$G
    PSModulePath=C:\Program Files\WindowsPowerShell\Modules;C:\windows\system32\WindowsPowerShell\v1.0\Modules;c:\Program Files\Intel\Wired Networking\
    PTSMINSTALLPATH=c:\Program Files\HP\HP ProtectTools Security Manager\Bin\
    PTSMINSTALLPATH_X86=c:\Program Files (x86)\HP\HP ProtectTools Security Manager\Bin\
    PUBLIC=C:\Users\Public
    RegionCode=NA
    SESSIONNAME=Console
    SystemDrive=C:
    SystemRoot=C:\windows
    TEMP=C:\Users\Freddy\AppData\Local\Temp
    TMP=C:\Users\Freddy\AppData\Local\Temp
    windir=C:\windows
    XDCROOT=C:\ti\xdctools_3_50_05_12_core
    *********************************************************************************************************************************************************************

    When i try to create projects using pdkCreateProject results:

    It looks like the PDK_SHORTNAME is wrong, i haven't messed with the script
    where can this be fixed

    C:\ti\pdk_k2hk_4_0_9\packages>pdkProjectCreate.bat K2K
    =========================================================================
    Configuration:
    SOC : K2K
    BOARD : all
    ENDIAN : little
    MODULE : all
    PROJECT_TYPE : all
    PROCESSOR : arm
    PDK_SHORT_NAME : C:\ti\PDK_K2~2\packages\
    =========================================================================
    Checking Configuration...
    Complete
    =========================================================================
    PDK_PARTNO : TCI6638
    PDK_ECLIPSE_ID : com.ti.pdk.k2hk
    RTSC_PLATFORM_NAME : ti.platforms.evmTCI6638K2K
    RTSC_TARGET : gnu.targets.arm.A15F
    CCS_DEVICE : "Cortex A.TCI6638K2K"
    *****************************************************************************
    Detecting all projects in PDK and importing them in the workspace C:\ti\PDK_K2~2\packages\\MyExampleProjects
    Detected Test Project: cppiK2KArmBiosTestProject
    The system cannot find the path specified.
    Copying macro.ini
    The system cannot find the path specified.
    0 file(s) copied.
    Detected Test Project: PA_emacExample_K2KArmBiosExampleProject
    The system cannot find the path specified.
    Copying macro.ini
    The system cannot find the path specified.
    0 file(s) copied.
    Detected Test Project: PA_UnitTest_K2KArmBiosTestProject
    The system cannot find the path specified.
    Copying macro.ini
    The system cannot find the path specified.
    0 file(s) copied.
    Detected Test Project: qmInfraK2KArmBiosExampleProject
    The system cannot find the path specified.
    Copying macro.ini
    The system cannot find the path specified.
    0 file(s) copied.
    Detected Test Project: qmAccK2KArmBiosTestProject
    The system cannot find the path specified.
    Copying macro.ini
    The system cannot find the path specified.
    0 file(s) copied.
    Detected Test Project: qmDCfgK2KArmBiosTestProject
    The system cannot find the path specified.
    Copying macro.ini
    The system cannot find the path specified.
    0 file(s) copied.
    Detected Test Project: qmDescK2KArmBiosTestProject
    The system cannot find the path specified.
    Copying macro.ini
    The system cannot find the path specified.
    0 file(s) copied.
    Detected Test Project: qmInsRegionK2KArmBiosTestProject
    The system cannot find the path specified.
    Copying macro.ini
    The system cannot find the path specified.
    0 file(s) copied.
    Detected Test Project: qmQAllocK2KArmBiosTestProject
    The system cannot find the path specified.
    Copying macro.ini
    The system cannot find the path specified.
    0 file(s) copied.
    Detected Test Project: qmQosSchedCModelK2KArmBiosTestProject
    The system cannot find the path specified.
    Copying macro.ini
    The system cannot find the path specified.
    0 file(s) copied.
    Detected Test Project: qmQosSchedDropSchedK2KArmBiosTestProject
    The system cannot find the path specified.
    Copying macro.ini
    The system cannot find the path specified.
    0 file(s) copied.
    Detected Test Project: qmQosSchedK2KArmBiosTestProject
    The system cannot find the path specified.
    Copying macro.ini
    The system cannot find the path specified.
    0 file(s) copied.
    Detected Test Project: qmQosSchedWideK2KArmBiosTestProject
    The system cannot find the path specified.
    Copying macro.ini
    The system cannot find the path specified.
    0 file(s) copied.
    Detected Test Project: qmQosTestK2KArmBiosTestProject
    The system cannot find the path specified.
    Copying macro.ini
    The system cannot find the path specified.
    0 file(s) copied.
    Detected Test Project: qmSCfgK2KArmBiosTestProject
    The system cannot find the path specified.
    Copying macro.ini
    The system cannot find the path specified.
    0 file(s) copied.
    Detected Test Project: qmSrioContextK2KArmBiosTestProject
    The system cannot find the path specified.
    Copying macro.ini
    The system cannot find the path specified.
    0 file(s) copied.
    Detected Test Project: qmSrioRtrK2KArmBiosTestProject
    The system cannot find the path specified.
    Copying macro.ini
    The system cannot find the path specified.
    0 file(s) copied.
    Detected Test Project: SA_BasicExample_K2KArmBiosExampleProject
    The system cannot find the path specified.
    Copying macro.ini
    The system cannot find the path specified.
    0 file(s) copied.
    Detected Test Project: SA_BasicExample_w3gpp_K2KArmBiosExampleProject
    The system cannot find the path specified.
    Copying macro.ini
    The system cannot find the path specified.
    0 file(s) copied.
    Detected Test Project: SA_UnitTest_K2KArmBiosTestProject
    The system cannot find the path specified.
    Copying macro.ini
    The system cannot find the path specified.
    0 file(s) copied.
    Detected Test Project: SA_UnitTest_w3gpp_K2KArmBiosTestProject
    The system cannot find the path specified.
    Copying macro.ini
    The system cannot find the path specified.
    0 file(s) copied.
    Detected Test Project: NIMU_emacExample_EVMK2K_armBiosExampleProject
    The system cannot find the path specified.
    Copying macro.ini
    The system cannot find the path specified.
    0 file(s) copied.
    No projects detected
    Project generation complete
    *****************************************************************************
  • 1. Still i cant find TOOLS_INSTALL_PATH on your environment variables.

    2. Another suggestion would be to re-install the Processor SDK and try again.()

    Thank you.