This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bad inittab entry at line 5

Hello!

I have a problem as shown below:

VFS: Mounted root (jffs2 filesystem) on device 31:11.
Freeing init memory: 144K
init started: BusyBox v1.13.2 (2010-06-21 12:46:04 IST)
Bad inittab entry at line 5
can't open /dev/si: No such file or directory
can't open /dev/~~: No such file or directory
can't open /dev/l0: No such file or directory
can't open /dev/l1: No such file or directory
can't open /dev/l2: No such file or directory
can't open /dev/l3: No such file or directory
can't open /dev/l4: No such file or directory
can't open /dev/l5: No such file or directory
can't open /dev/l6: No such file or directory
can't open /dev/z6: No such file or directory
can't open /dev/S: No such file or directory
can't open /dev/1: No such file or directory
process '/sbin/sulogin' (pid 1040) exited. Scheduling for restart.
process '/sbin/getty 115200 ttyS0' (pid 1041) exited. Scheduling for restart.
process '/sbin/getty 38400 tty1' (pid 1042) exited. Scheduling for restart.

I use DVSDK_3_10 on my  DM36X EVM board, and the rootfs is extract from arago-demo-image-dm365-evm.tar.gz . All the software resource are download from TI website , it should not be anything wrong.