This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TMS320DM8148: If mmc does not support CMD56 option, then kernel will continuously throw error

Part Number: TMS320DM8148


Tool/software: Linux

I have TI's DM8148 based board,

I want to get wear level of SD card by sending CMD56 opcode to MMC using IOCTL. I am able to get correct response from some SD card if they have support of CMD56.

But for those SD card, who do not have support of CMD56 , I got continuous error logs, and then system slows down. 

I want to get rid of continuous error logs, is there any patch in kernel which will remove that thing ?

Currently My board has kernel 2.6.37 version. Attaching error log file for reference.

Thanks,

Harshil

kernel_logs (1).txt