This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/BEAGLEBK: NFS setup fails

Part Number: BEAGLEBK

Tool/software: Linux

With PROCESSOR-SDK-LINUX-AM335X  04_03_00_05

Write following information to microSD card on the Beaglebone:

setenv serverip 192.168.1.104
setenv rootpath /home/tim/ti-processor-sdk-linux-am335x-evm-04.03.00.05/targetNFS
setenv bootfile zImage
setenv ip_method dhcp
setenv nfs_bootfile 'nfs ${loadaddr} ${serverip}:${rootpath}${bootdir}/${bootfile}'
setenv nfs_fdtfile 'nfs ${fdtaddr} ${serverip}:${rootpath}${bootdir}/${fdtfile}'
setenv bootcmd 'setenv autoload no; dhcp; run nfs_bootfile; run findfdt; run nfs_fdtfile; run netargs; bootz ${loadaddr} - ${fdtaddr}'

Reboot the board, then failed to connect NFS:

NAND:  0 MiB
MMC:   OMAP SD/MMC: 0
reading uboot.env
Net:   cpsw, usb_ether
Hit any key to stop autoboot:  0
link up on port 0, speed 100, full duplex
BOOTP broadcast 1
BOOTP broadcast 2
DHCP client bound to address 192.168.1.105 (998 ms)
link up on port 0, speed 100, full duplex
###############################################################T ##
       .........

         ###########################################################T T T T T
done
Bytes transferred = 3627816 (375b28 hex)
link up on port 0, speed 100, full duplex
########T T T T T T

The file was transferred completely, but NFS setup failed. Need help.

Thank you.

Tim