This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Champs,
Hardware: AM3358+TPS65217D
Software: TI_Android_GingerBread_2_3_4_AM335x_Sources
Question: In the deep sleep, press power key, the system is waken up, but then the system enters the sleep mode again.
The initial reason customer guessed: The kernel was waken up and generate the "input" event, but the event can't be captured by the application level which caused to fail to get the wakeup lock and then the system re-enter the sleep mode.
Below is the log:
[ 85.169982] PM: suspend of devices complete after 11.560 msecs
[ 85.172027] PM: late suspend of devices complete after 1.982 msecs
[ 636.250305] GFX domain entered low power state
[ 636.250366] Successfully transitioned all domains to low power state
[ 636.459381] PM: early resume of devices complete after 208.355 msecs
[ 636.459808] lj hx8357_bl_init on:1
[ 636.460021] android_work: sent uevent USB_STATE=DISCONNECTED
[ 636.474884] android_work: sent uevent USB_STATE=CONNECTED
[ 636.482086] android_work: sent uevent USB_STATE=DISCONNECTED
[ 636.543731] android_work: sent uevent USB_STATE=CONNECTED
[ 636.553375] gadget: high-speed config #1: android
[ 636.553649] android_work: sent uevent USB_STATE=CONFIGURED
[ 636.660858] gpio_keys_resume
[ 636.682678] PM: resume of devices complete after 43.811 msecs
[ 636.761077] xs >>>>>>>>>>>>>>> gpiod keys_func
[ 636.765899] Restarting tasks ...
[ 636.772247] adb_release
[ 636.775909] adb_open
[ 636.788635] wakeup wake lock: PowerManagerService
[ 636.809478] done.
[ 636.811676] suspend: exit suspend, ret = 0 (1970-01-03 00:21:11.131137580 UTC)
[ 636.937896] PM: Syncing filesystems ... done.
[ 636.979156] Freezing user space processes ... (elapsed 0.01 seconds) done.
[ 637.001892] Freezing remaining freezable tasks ... (elapsed 0.01 seconds) done.
[ 637.021820] lj hx8357_bl_init on:0
[ 637.059204] Suspending console(s) (use no_console_suspend to debug)
Thanks.
Rgds
Shine