Tool/software: TI-RTOS
Hello.
I executed the TIDL OD usecase with the sample input files supported from TI on the TDA2PX EVM board, but it was not proceed after the following message displayed.
Can you guess what happend?
[IPU1-0]
[IPU1-0] TIDL Usecases
[IPU1-0] ---------------
[IPU1-0] 1: TIDL File I/O Usecase
[IPU1-0] 2: Semantic Segmentation Usecase
[IPU1-0] 3: TIDL OD Usecase
[IPU1-0]
[IPU1-0] x: Exit
[IPU1-0]
[IPU1-0] Enter Choice:
[IPU1-0]
[IPU1-0] 45.748124 s:
[IPU1-0] 47.552491 s: FILE: Reading file [inHeader_OD] ...
[IPU1-0] 47.559903 s: FILE: File read Done. [12000 bytes]
[IPU1-0] 47.589123 s: DECODE: Create in progress ... !!!
[IPU1-0] 47.844872 s: DECODE: Creating CH0 of 768 x 320 [1] [0],target bitrate = 10000 Kbps ...
[IPU1-0] 47.845726 s: DECODE: All CH Create ... DONE !!!
[IPU1-0] 47.847739 s: DECODE: Create ... DONE !!!
[IPU1-0] 47.848136 s: VPE: Create in progress !!!
[IPU1-0] 47.942292 s: VPE: Loading Down-scaling Co-effs
[IPU1-0] 47.942505 s: VPE: Co-effs Loading ... DONE !!!
[IPU1-0] 47.942719 s: VPE: Create Done !!!
[IPU1-0] 47.943786 s: IPC_OUT_0 : Create in progress !!!
[IPU1-0] 47.944152 s: IPC_OUT_0 : Create Done !!!
[IPU1-0] 47.952632 s: SYSTEM: NOTIFY: [EVE4] is NOT ENABLED in this build !!!
[IPU1-0] 47.952723 s: Assertion @ Line: 199 in system_ipc_bios_ipc.c: (Bool)FALSE : failed !!!
[IPU1-0] 47.953150 s: Assertion @ Line: 199 in system_ipc_bios_ipc.c: (Bool)FALSE : failed !!!
[HOST ] 47.944335 s: IPC_IN_0 : Create in progress !!!
[HOST ] 47.944641 s: IPC_IN_0 : Create Done !!!
[HOST ] 47.944763 s: ALGORITHM: Create in progress (algId = 12) !!!
[HOST ] 47.952388 s: UTILS: DMA: Allocated CH (TCC) = 0 (0)
[HOST ] 47.952418 s: UTILS: DMA: 0 of 1: Allocated PaRAM = 0 (0x43305600)
[HOST ] 47.952418 s: ALGORITHM: Create Done (algId = 12) !!!
[HOST ] 47.952540 s: IPC_OUT_3 : Create in progress !!!
[HOST ] 47.952571 s: IPC_OUT_3 : Create Done !!!