Other Parts Discussed in Thread: TMS320C6745, TLV320AIC3007
We have a medical device which uses the TMS320C6745 DSP. The device also contains a Telit chip for cell communications which we are upgrading to a newer chip. With the newer cell chip and antenna, we noticed that we now have spurious signals from the McASP MCLK. connected to a TLV320AIC3007 codec which degrades the cell signal. The McASP is configured and initialized in the power on sequence. However, we don't need the audio when transmitting data via the cell chip, so we would like to turnoff the MCLK while transmitting and then turn it back on when done. We have a hardware solution but prefer to do this in software. Is this something that can be done and if so how?