Other Parts Discussed in Thread: TVP5150
Hello All,
I would like to ask question on digital camera resolution:
I have seen many cameras saying in their description that they support both:
628 x 582 (PAL)
510 x 492 (NTSC)
I am a little bit confused. Because according to ITU BT.656, for PAL TV, the digital sampling rate is:
-
50 fields/second
-
864 samples per line, 720 of them are active
-
480 out of 525 lines in a frame (two fields) are active.
But all of these are different with 628 x 582 standards above. Do these cameras conform to BT.656 standard? Do they output digital or analog signals (for example, composite video signal)? Does the resolution (628 x 582) refer to density of subpixel sensors in the sensor array? If so, does it refer to the active/valid area of the sensor array or the entire area?
Another question is on the frame of digital camera:
-
PAL has 50 fields (25 frames) per second
-
NTSC has 60 fields (30 frames) per second
So how can camera support both standards? Does it have to switch internally its clock rate, altering the image area size, as well as doing Digital-to-Analog conversion at a different rate?
These questions vexed me for qutie a few days. I would sincerely appreciate anyone who would give the right answer.
Thanks,
Jim