Part Number: TDA2EXEVM
Tool/software: Linux
Dear Sirs:
We are using the Linux Environment of VSDK 03_02_00_00.
And We try to use Alg_VpeSwMs.
Base on the URL:
processors.wiki.ti.com/.../StdDotH
When try to write code use the AlgVpeSwMs, we add the following into the Linux MAKEFILE
-Dxdc_target_types__=gnu/targets/arm/std.h -Dxdc_target_name__=GCArmv7A
But we found it will cause error because the XDC tool only contains the core part but no other parts like xdctools_3_25_05_94 we used in DM81xx.
My question is which version of XDC tools we should use if we are going to create the VpeSwMs link in Linux APP.
Regards,
/ckhsu