Hello,
I ma using ICEAM3359 from TI and I managed to create my project and also build the demo. There are a couple of issues I am facing in executing the demo. This is kind of urgent as I have to show it to my professor who is a very sweet guy and has gone above and beyond to get a funding for our industrial automation project. So when I build the full project, it gives me errors. After referring to the guide, it asks me to patch the source files which I don't have . I don't know how to patch and what to patch and where to include those files after patching? Do I simply replace the old files from the full slave project create through the TI given bat file? Here it is confusing.
Secondly, the guide says flashing the project on an SD card or directly on the processor. Currently my SD Card has the RTOS image. Do you want me to include the Project file on the SD card or simply flash the board through CCS?
Third problem is TwinCAT3 is not recognising my board. It recognises the ethernet connection which is existing with the PC but after following the guide which says to relaod devices, I somehow don't get any desirable response. I cannot scan boxes. I think this is directly related to flashing the processor or the sd card, but I am not sure. Any help in that regard would be very beneficial.
Please help me out with these questions. I have a couple more, but if these get solved, I can ask further. Thanks a lot and much appreciation for your selfless help!