Other Parts Discussed in Thread: TPS65217
Tool/software: Linux
Hello Friends
I am getting this problem with Buildroot.
Starting network: udhcpc: started, v1.27.2
[ 2.928374] net eth0: initializing cpsw version 1.12 (0)
[ 2.933951] net eth0: initialized cpsw ale version 1.4
[ 2.939382] net eth0: ALE Table size 1024
[ 2.945195] libphy: PHY 4a101000.mdio:00 not found
[ 2.950239] net eth0: phy "4a101000.mdio:00" not found on slave 0, err -19
[ 2.957426] libphy: PHY 4a101000.mdio:01 not found
[ 2.962456] net eth0: phy "4a101000.mdio:01" not found on slave 1, err -19
[ 2.980308] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
udhcpc: sending discover
udhcpc: sending discover
udhcpc: sending discover
udhcpc: no lease, failing
Failed to bring up eth0.
FAIL
Starting dhcpcd...
no interfaces have a carrier
forked to background, child pid 149
Starting Network Interface Plugging Daemon: eth0.
Starting ntpd: OK
Starting dropbear sshd: [ 12.722674] random: dropbear: uninitialized urandom read (32 bytes read, 29 bits of entropy available)
OK
Starting vsftpd: OK
Welcome to Buildroot
buildroot login: root
Password:
# ifconfig
eth0 Link encap:Ethernet HWaddr E8:EB:11:28:E6:73
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Interrupt:174
The IP does not get assigned and I have power reboot my system couple of times to get the IP assignment.
I am using 4.4.41 kernel version and glibc.