This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6467T encodedecode Demo Crashes After Few Minutes



I updated to DVSDK 3.10.00.19 and ran the encodedecode demo program.  The board ran for  about more than 3 minutes and reset.

root@dm6467t-evm:/opt/dvsdk/dm6467# ./loadmodules.sh
CMEMK module: built on Oct 22 2010 at 13:30:38
   Reference Linux version 2.6.32
   File /home/tochau/dvsdk/dvsdk_3_10_00_19/linuxutils_2_25_04_10/packages/ti/sdo/linuxutils/cmem/src/module/cmemk.c allocated heap buffer 0xc9000000 of size 0x99000 cmemk initialized
DSPLINK Module (1.64) created on Date: Oct 22 2010 Time: 13:29:10
root@dm6467t-evm:/opt/dvsdk/dm6467# 
root@dm6467t-evm:/opt/dvsdk/dm6467# ./encodedecode
Encodedecode demo started.
Encode Decode demo ARM Load: 13% DSP Load: 100% Display Type: 720P 60Hz Video Codec: H.264 BP Video fps: 22 fps Video bit rate: 677 kbps Video resolution: 1280x720 Time: 00:00:01  
Encode Decode demo ARM Load: 10% DSP Load: 88% Display Type: 720P 60Hz Video Codec: H.264 BP Video fps: 30 fps Video bit rate: 361 kbps Video resolution: 1280x720 Time: 00:00:02  

...

Booting PSP Boot Loader 

Starting NAND Copy 

Booting Application @ 0x81080000  

U-Boot 2009.08-00002-gcab1855 (Jan 20 2010 - 04:20:31) 

I2C:   ready
DRAM:  256 MB
NAND:  128 MiB
In:    serial
Out:   serial
Err:   serial
ARM Clock :- 495MHz
DDR Clock :- 396MHz
Net:   Ethernet PHY: GENERIC @ 0x01 DaVinci EMAC Hit any key to stop autoboot:  3  2  1  0  Using DaVinci EMAC device
TFTP from server 192.168.2.100; our IP address is 192.168.2.223
Filename 'uImage'.
Load address: 0x80700000
Loading: *#################################################################      #################################################################      ########### done

Bytes transferred = 2066204 (1f871c hex)
## Booting kernel from Legacy Image at 80700000 ...
    Image Name:   Linux-2.6.32-rc2-davinci1
    Image Type:   ARM Linux Kernel Image (uncompressed)
    Data Size:    2066140 Bytes =  2 MB
    Load Address: 80008000
    Entry Point:  80008000
    Verifying Checksum ... OK
    Loading Kernel Image ... OK
OK 
Starting kernel ... 
Uncompressing Linux....................................................................................................................................... done, booting the kernel. 
Booting PSP
Boot Loader  Starting
NAND Copy  Booting Application @ 0x81080000   U-Boot 2009.08-00002-gcab1855 (Jan 20 2010 - 04:20:31)  I2C:

 

The kernel was uncompressed but it could not run.

What's the problem?  Please help!  Thank you.