This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3358: Yocto build issue

Part Number: AM3358

Im using YOCTO SDK 8 and I have such build configuration:

Build Configuration:
BB_VERSION = "1.22.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-14.04"
TARGET_SYS = "arm-oe-linux-gnueabi"
MACHINE = "mtax_am335x"
DISTRO = "arago"
DISTRO_VERSION = "2015.02"
TUNE_FEATURES = "armv7a vfp thumb neon callconvention-hard cortexa8"
TARGET_FPU = "vfp-neon"
meta-elesy-tc71x-common = "<unknown>:<unknown>"
meta-arago-distro
meta-arago-extras = "amsdk-08.00.00.00-integration:2d15e7da62646c907d24942483cbfddc03a6310b"
meta-qt5 = "(detachedfrom37e921d):37e921db22689131144b453d53a8cce4a314aa48"
toolchain-layer
meta-networking
meta-ruby
meta-oe = "(detachedfromd3d14d3):d3d14d3fcca7fcde362cf0b31411dc4eea6d20aa"
meta-ti = "amsdk-08.00.00.00-integration:4fc5c40602d9a826661934a94a8a7e5e5864c88f"
meta-linaro-toolchain = "(detachedfrombc63e77):bc63e777ad2748b8bfa7fa70ffd74700fa21a567"
meta = "(detachedfromf34de21):f34de2175f1d6a443f219b8ceaaf796cfbc6efd5"

After I`ve changed build configuration to PROCESSOR SDK 04.02.00.09 I have such one:

Build Configuration:
BB_VERSION = "1.32.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "DebianGNULinux-7"
TARGET_SYS = "arm-linux-gnueabi"
MACHINE = "am335x-esom"
DISTRO = "arago"
DISTRO_VERSION = "2017.10"
TUNE_FEATURES = "arm armv7a vfp thumb neon callconvention-hard"
TARGET_FPU = "hard"
meta-elesy = "master:0454f792997031d8f4b2244a1aad59c01f74b89a"
meta-processor-sdk = "HEAD:eaac60268857bc56bf89625df93935a272b63341"
meta-ros = "HEAD:e01c6ace0d4f9d700449edad3781e9cd505b5e10"
meta-arago-distro
meta-arago-extras = "HEAD:d34c861f846f35d089e1caf224ec43079be7b202"
meta-browser = "HEAD:26d50665e2f7223c5f4ad7481a8d2431e7cb55fb"
meta-openamp = "HEAD:8a214032bfb7e8124bc1485c70c69f7d60abb819"
meta-qt5 = "HEAD:2c9f0e4eb0e9097f6f872ec1e1d81768a8ab5f1b"
meta-networking
meta-ruby
meta-python
meta-oe
meta-gnome
meta-multimedia = "HEAD:b40116cf457b88a2db14b86fda9627fb34d56ae6"
meta-ti = "HEAD:351ccf1928a18c2b69fd19b09b980c9aa3af2e26"
meta-linaro-toolchain
meta-optee = "HEAD:5d2cb685217794293ea2bab18d7e62019c329d06"
meta = "HEAD:1718f0a6c1de9c23660a9bebfd4420e3c4ed37e6"

And all things include U-Boot spl cant start - nothing happen even when I`ve xmodem SPL part u-boot to board.

I suspect TARGET_FPU = "hard" settings a fail reason.

How can I turn TARGET_FPU settings to good?