Tool/software: Linux
Hello,
I am running PROCESSOR_SDK_VISION_03_01_00_00 Linux on the tda2evm5777 and I am having an issue when I try to run it on another hardware (Part 1 below). I also tried to recreate the issue on the tda2evm5777 hardwaren(see part 2).
Part 1
Linux starts to boot but will stop after these print statements:
[ 2.653974] dmm 4e000000.dmm: initialized all PAT entries
[ 2.661366] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 2.668038] [drm] No driver support for vblank timestamp query.
[ 2.674367] [drm] Initialized omapdrm 1.0.0 20110917 on minor 0
[ 2.693383] pcf857x: probe of 0-0020 failed with error -121
[ 2.699149] pcf857x: probe of 0-0021 failed with error -121
[ 2.705199] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 2.824026] asoc-simple-card sound0: tlv320aic3x-hifi <-> 48468000.mcasp mapping ok
[ 2.846947] omap_hsmmc 480d1000.mmc: card claims to support voltages below defined range
[ 2.856117] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 2.861575] hctosys: unable to open rtc device (rtc0)
[ 2.875008] evm_1v8: disabling
[ 2.878099] aic_dvdd: disabling
[ 2.881432] ldousb: disabling
[ 2.884702] pbias_mmc_omap5: disabling
[ 2.888628] ALSA device list:
[ 2.891624] #0: DRA7xx-EVM
[ 2.895222] Waiting for root device PARTUUID=adadfbee-02...
[ 2.906404] mmc1: queuing unknown CIS tuple 0x91 (3 bytes)
[ 2.912637] mmc1: new high speed SDIO card at address 0001
Part 2
I tried to recreate the issue on the evaluation board (tda2evm5777) by disabling i2c1 in the dra7-evm-common.dts file. we can create a similar boot up halt. Here are the ending print statements for that:
[ 2.261911] Power Management for TI OMAP4+ devices.
[ 2.267080] Registering SWP/SWPB emulation handler
[ 2.274549] dmm 4e000000.dmm: initialized all PAT entries
[ 2.295529] omapdss_dss 58000000.dss: master bind failed: -517
[ 2.302038] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 2.307889] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr25 mode
[ 2.314316] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr12 mode
[ 2.433424] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 2.439631] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 2.445917] ti_oppdm 4a003b20.oppdm: Unable to get vdd regulator:-517
[ 2.453691] omapdss_dss 58000000.dss: master bind failed: -517
[ 2.461362] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 2.469302] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr25 mode
[ 2.475754] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr12 mode
[ 2.483051] hctosys: unable to open rtc device (rtc0)
[ 2.501201] evm_1v8: disabling
[ 2.504305] evm_3v3_sw: disabling
[ 2.507636] aic_dvdd: disabling
[ 2.510794] pbias_mmc_omap5: disabling
[ 2.514580] vmmcwl_fixed: disabling
[ 2.518280] ALSA device list:
[ 2.521259] No soundcards found.
[ 2.525593] Waiting for root device PARTUUID=adadfbee-02...
Questions
- What is Linux trying to do or waiting on that would make it pause at this point in the bootup sequence?
- Does Linux require ECC DDR?
- Why would disabling I2C1 on a Vayu result in a similar boot halt?
Please let me know if you need any information. I can also provide more boot print statements if it helps.
Thank you in advance!
-iFer