This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM36X EVM caputure from IMAGE INTERFACE

I try to obtain the image by the image interface on DM36X EVM.

First of all, sample program (examples-davinci.tar.gz) was obtained on the following page.
http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/dvsdk/DVSDK_3_10/latest/index_FDS.html

examples-davinci.tar.gz was defrosted, and make did "examples-r37/imp-prev-rsz/dm365/capture_prev_rsz_onthe_fly_bayer.c".

It becomes an error because of the following calls if it executes it.
ioctl (fdCapture, VIDIOC_S_INPUT, &input.index)

The following messages are displayed in the console.

-----

davinci_resizer davinci_resizer.2: RSZ_G_CONFIG:1:1:196

input_std_paradavinci_previewer davinci_previewer.2: ipipe_set_preview_config
ms: name = V4L2_STD_MT9T001_VGA_30FPS
input_stddavinci_previewer davinci_previewer.2: ipipe_set_preview_config
_params: output width = 720
calling cmem utilities for allocating frame buffers
Allocating capture buffers :buf size = 2621440
Got 0x403e4000 from CMEM, phy = 0x87b00000
Got 0x40664000 from CMEM, phy = 0x87880000
Got 0x408e4000 from CMEM, phy = 0x87600000
Allocating display buffers :buf size = 2621440
Got 0x40b64000 from CMEM, phy = 0x87380000
Got 0x40de4000 from CMEM, phy = 0x87100000
Got 0x41064000 from CMEM, phy = 0x86e80000
opening resize device
Successfully set mode to single shot in resizer
Setting default configuration in Resizer
default configuration setting in Resizer successfull
default values at driver
rsz_ss_config.output1.enable = 1
rsz_ss_config.output1.width  = 640
rsz_ss_config.output1.height = 480
rsz_ss_config.output2.enable = 1
rsz_ss_config.output2.width  = 640
rsz_ss_config.output2.height = 480
Changing output width to 640
Changing output height to 480
Resizer initialized
Operating mode changed successfully to continuous in previewerSetting default configuration in previewer
default configuration setting in previewer successfull
Setting default for LUT Defect Correction
Setting default for OTF Defect Pixel Correction
Setting default for 2-D Noise filter - 1
Setting default for 2-D Noise filter - 2
Setting default for Green Imbalance Correction
Setting default for White balance
Setting default for CFA Interpolation
Setting default for RGB-RGB Conversion - 1
Setting default for Gamma Correction
Setting default for RGB-RGB Conversion - 2
Setting default for 3D LUT
Setting default for RGB-YCbCr conversion
Setting default for Global Brightness,Contrast Control
Setting default for YUV 422 conversion
Setting default for Luminance Adjustment
Setting default for Edge Enhancer
Setting default for Chromatic Artifact Reduction
Setting default for Chromatic Gain Suppression
previewer initialized
setting data format
set_data_format:setting std to 0
input.name = Composite
input.name = S-Video
input.name = Component
input.name = Camera
Camera 3
ioctl:VIDIOC_S_INPUT failed
: Invalid argument
SetDataFormat failed

-----

Are some settings necessary?

 

Regards,