Hello,
I can't build the examples, provided with the XDAIS package for the DM365 device. I work with XDAIS 6.25.01.08, XDC tools 3.16.02.32 and CCS v4 (CGT 4.6.3.0). I followed the build instructions provided with the examples. After executing gmake, the build process starts and makes the '.interfaces' steps for all examples, but the build process stops after the first '.libraries' step with the error message:
The following symbols are undefined: _AUDDECCOPY_TI_IAUDDECCOPY
1 Assembly Error, No Assembly Warnings
Errors in Source - Assembler Aborted
I think I've made the correct changes for the config.bld and the Makefile. Here are my changes:
config.bld
var target = xdc.module('ti.targets.arm.elf.Arm9');
target.rootDir = 'C:/Programme/Texas Instruments/ccsv4/tools/compiler/tms470';
Build.targets.$add(target);
Makefile
XDC_INSTALL_DIR = C:/Programme/Texas Instruments/xdctools_3_16_02_32
XDAIS_INSTALL_DIR = C:/Programme/Texas Instruments/xdais_6_25_01_08
XDCPATH = ^;$(XDAIS_INSTALL_DIR)/packages;$(XDC_INSTALL_DIR)/packages;
To start the build process, I changed to the examples directory and enter 'gmake clean' and then 'gmake'.
Any help would be great! Thanks!