Is it possible to use one of the TSIF outputs in this EVM through the daughter card expansion?
I mean, if I take the corresponding pins of the UART0 / Video Output on the DC, is there a manner to tell the onboard CBT mux isolate it from the rest of the circuit after CBTs?
Is just simply not to use the port as a UART/Video Out and use it as a TSIF output in (MV)Linux?
(fell free to ask for clarifications)
thanks.