Hi,
We have developed a custom board using TMS320C6746. We are using SPI Flash for boot purposes. Now we want to program the flash from a PC and through UART. We connected a SPI Flash to the 6748 EVM and using 'sfh_OMAP_L138' utility, we could program the SPI Flash. But it seems the utility uses UART2 for the purpose. Now using the same utility can we program the flash through UART 0 with a C6746 DSP as we are using UART2 for other purposes.
regards,
Vasudevan OM