Other Parts Discussed in Thread: OMAP3530
Hi all,
I have read many discussion, websites, documents, but I still don't understand DSPLINK Memory Map in detail, espectially about POOL, CHANNEL. Can anybody help me to understand it much more. In my config/all/CFG_OMAP3530_SHMEM.c:
#define CODEENTRYID 1u
#define CODEMEMORYADDR (RESETCTRLADDR + RESETCTRLSIZE)
#define CODEMEMORYSIZE 0xFFF80u
#define SHAREDENTRYID0 2u
#define SHAREDMEMORYADDR0 (CODEMEMORYADDR + CODEMEMORYSIZE)
#define SHAREDMEMORYSIZE0 0x5000u
#define SHAREDENTRYID1 3u
#define SHAREDMEMORYADDR1 (SHAREDMEMORYADDR0 + SHAREDMEMORYSIZE0)
#define SHAREDMEMORYSIZE1 0x2B000u
#define POOLENTRYID 4u
#define POOLMEMORYADDR (SHAREDMEMORYADDR1 + SHAREDMEMORYSIZE1)
#define POOLMEMORYSIZE 0x000D0000u
STATIC LINKCFG_Pool LINKCFG_poolTable_00 [] =
{
{
"SMAPOOL", /* NAME : Name of the pool */
SHAREDENTRYID1, /* MEMENTRY : Memory entry ID (-1 if not needed) */
(Uint32) 0x70000, /* POOLSIZE : Size of the pool (-1 if not needed) */
(Uint32) -1, /* IPSID : ID of the IPS used */
(Uint32) -1, /* IPSEVENTNO : IPS Event number associated with POOL */
POOLENTRYID, /* POOLMEMENTRY : Pool memory region section ID */
0x0, /* ARGUMENT1 : First Pool-specific argument */
0x0 /* ARGUMENT2 : Second Pool-specific argument */
}
} ;
What exactly are the MEMENTRY and the POOLENTRYID? When I call function POOL_open(), where will buffers will be allocated? by doing practice, I see that the total memory required by POOL_open() is limited by POOLMEMORYSIZE. So I guess that all buffers will be located in POOLENTRYID. Is that true? If that, I really don't understand the responsibility of the MEMENTRY (SHAREDENTRYID1)?
I also wonder about CHNL_allocateBuffer() function. When this function is called, where will the buffers be allocated? In POOL or in HEAP?
/dsp/inc/DspBios/5.XX/OMAP3530/dsplink-omap3530-base.tci
/* ============================================================================
* MEM : Adjust DDR2
* ============================================================================
*/
var DDR2 = prog.module("MEM").instance("DDR2");
DDR2.base = RESET_VECTOR.base + RESET_VECTOR.len ;
DDR2.len = 0x000FFF80;
DDR2.space = "code/data";
DDR2.createHeap = true;
DDR2.heapSize = 0x10000;
DDR2.comment = "DDR2";
With this configuration, is Heap in DDR2 memory? What is the relation between DDR2.len and DDR2.heapSize?
Can anybody help me to figure out?
I deeply thank you! :)
(My English is not good. So, if there is anything bother you, please let me know, I will describe it more clearly. Sorry for any convinience! )