This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Load from SPI flafh

Hello.
I made a device based on C5535.
When running through the XDS-100 debugger, everything is fine.
When running with a flush, the C5535 reads the program code, but then does not work. I draw a conclusion about it by GPIO17 IP-Phone_DSP(2x_Channel)(Ver. 1.00).sch


/**
 * main.c
 */
/* ANSI C headers */
#include <stdlib.h>
#include <stdio.h>
#include <string.h>
#include "csl_intc.h"

/* System definitions and utilities */
#include <ti/mas/types/types.h>

/* AER, DRC, AGC, MSS and BF header files */
#include <ti/mas/aer/aer.h>
#include <ti/mas/aer/agc.h>
#include <ti/mas/aer/drc.h>
#include <ti/mas/aer/mss.h>
#include <ti/mas/aer/bf.h>
#include "device.h"

/* AER simulation constants and data structures */
#include <ti/mas/aer/test/aersim/aersim.h>
#include <ti/mas/aer/test/aersim/aerbuffs.h>

/* SIU simulation header files */
#include <ti/mas/aer/test/siusim/siu.h>
#include <ti/mas/aer/test/siusim/siuloc.h>
#include <ti/mas/aer/test/siusim/siuaer.h>
#include <ti/mas/aer/test/siusim/siubf.h>
#include <ti/mas/aer/test/piusim/piuloc.h>

#define AER_SIM_PEAK_MIPS_ERLE_THRESH 10
#define AER_SIM_DURATION_CONVERGED    3000 /* Run 30 seconds after converged */

/* Global structures for AER simulation */
siuSetup_t siuSetup;        /* simulation setup/configuration structure */
siuInst_t  siu_inst;        /* system integration unit (SIU) instance structure */
piuInst_t  piu_inst;        /* PCM interface unit (PIU) instance structure */
aepSimInst_t aepSimInst;    /* Acoustic echo path (AEP) simulator structure */
//aersimFileIO_t  aersim_fio; /* File I/O structure */
//sgnInstBuf_t sgnTxInst[AER_SIM_NUM_MIC]; /* Signal Generator (SGN) for Tx path (Near End) */
//sgnInstBuf_t sgnRxInst;                  /* Signal Generator (SGN) for Rx path (Far End)  */

/* Input and output buffers for AER simulation */
//linSample sim_data_rx_in    [SIU_AER_MAX_FRAME_LENGTH];
linSample sim_data_rx_out   [SIU_AER_MAX_FRAME_LENGTH];
linSample sim_data_dac      [SIU_AER_MAX_FRAME_LENGTH];  /* signal to D/A */
linSample sim_data_rx_sync  [SIU_AER_MAX_FRAME_LENGTH];  /* reference signal */
linSample sim_data_ne_speech[AER_SIM_NUM_MIC][SIU_AER_MAX_FRAME_LENGTH];
linSample sim_data_mic      [AER_SIM_NUM_MIC][SIU_AER_MAX_FRAME_LENGTH];
linSample sim_data_tx_in    [AER_SIM_NUM_MIC][SIU_AER_MAX_FRAME_LENGTH];
linSample sim_data_tx_out   [SIU_AER_MAX_FRAME_LENGTH];

#pragma DATA_ALIGN(bf_null, 4);
linSample bf_null[AER_SIM_NUM_MIC][SIU_AER_MAX_FRAME_LENGTH];

/* Buffers for loading or reading AER tail model coefficients */
#define NUM_H_VEC_GET 3
#define NUM_H_VEC_PUT 3
Fract aer_coef_mant[aer_NUM_WORDS_PER_H_VEC_16K*NUM_H_VEC_PUT];
tint aer_coef_exp[NUM_H_VEC_PUT];
aerTailModel_t aer_tail_model;

/* Buffers for reading BF filter coefficients */
Fract bf_filt_coef[AER_SIM_NUM_BF_MIC][bf_MAX_SUPPORTED_FILT_LEN];
tint bf_filt_len;

/* Prototypes of the funtions only referenced in this file */
//tbool aer_sim_fio_read_fe(aersimFileIO_t *fio, linSample *data_fe);
//tbool aer_sim_fio_read_ne(aersimFileIO_t *fio,
//                         linSample data_ne[][SIU_AER_MAX_FRAME_LENGTH],tint num_input);
//void aer_sim_fio_write_data(aersimFileIO_t *fio);
tint aer_sim_get_erle(siuInst_t *inst);
void aer_sim_print_version_mips(siuInst_t *inst);
void aer_sim_cfg_on_the_fly(siuInst_t *inst);

/* global variables for debugging purpose - to set conditional breakpoint */
Uint32 frm_cnt = 0;
int my_frm_cnt = 0;
int num_frames_converged = 0;




/******************************************************************************
 * FUNCTION PURPOSE: Get ERLE Measurement form AER
 *****************************************************************************/
tint aer_sim_get_erle(siuInst_t *inst)
{
  aerDebugStat_t aer_dbg;
  aerVersion_t aer_ver;

  /* get ERLE from the first mic */
  aerGetPerformance(inst->aerHFInst[0], &aer_dbg, &aer_ver, FALSE);

  return(aer_dbg.max_canc_l2);
} /* aer_sim_get_erle */

/******************************************************************************
 * FUNCTION PURPOSE: Simulate real time on-the-fly configuration/control of AER.
 *****************************************************************************/
void aer_sim_cfg_on_the_fly(siuInst_t *inst)
{
  int i;
  tint num_coeff_words, ret_code;

  /* Control AER: First, stop the program and change toggle_aer to TRUE. */
  if (siuSetup.toggle_aer) { /* --> break point can be set here to stop the code */
    /* Second, change aerCtl in Code Composer watch window to configure AER. */
    for(i=0; i<inst->phone_sys.num_HF_mic; i++){
      aerControl (inst->aerHFInst[i], (aerControl_t *)&siuSetup.aerCtl);
    }
    siuSetup.toggle_aer = FALSE;
  }

  /* Control AGC: First, stop the program and change toggle_agc to TRUE. */
  if (siuSetup.toggle_agc) { /* --> break point can be set here to stop the code */
    /* Second, change agcCtl in Code Composer watch window to configure AGC. */
    for(i=0; i<inst->phone_sys.num_HF_mic; i++){
      agcControl (inst->agcHFInst[i], (agcControl_t *)&siuSetup.agcCtl);
    }
    siuSetup.toggle_agc = FALSE;
  }

  /* Change SIU gains: follow same procedure as above */
  if (siuSetup.toggle_siugain) {
    for(i=0; i<inst->phone_sys.num_HF_mic; i++){
      siuGainControl (inst->agcHFhandles[i], (siuGainControl_t *)&siuSetup.siuGainCtl);
    }
    siuSetup.toggle_siugain = FALSE;
  }

  /* Read tail model filter from AER */
  if (siuSetup.toggle_getflt) {
    if(siuSetup.aer_kernel_srate == AER_SIM_SRATE_16000_DIV_8K) {
      num_coeff_words = aer_NUM_WORDS_PER_H_VEC_16K*NUM_H_VEC_GET;
    }
    else {
      num_coeff_words = aer_NUM_WORDS_PER_H_VEC_8K*NUM_H_VEC_GET;
    }
    ret_code = aerGetFilter(inst->aerHFInst[0], &aer_tail_model, &aer_coef_mant[0],
                            &aer_coef_exp[0], 0, num_coeff_words);
    if(ret_code != aer_NOERR) {
      //printf("Error when calling aerGetFilter with error code %d!\n", ret_code);
      exit(0);
    }

    for(i=0; i<siuSetup.system_cfg.num_BF_mic; i++)
    {
      ret_code = bfGetFilter(inst->bfInst, &bf_filt_coef[i][0], &bf_filt_len, bf_FG_BF, i);
      if(ret_code != bf_NOERR) {
        //printf("Error when calling bfGetFilter with error code %d!\n", ret_code);
        exit(0);
      }
    }

    siuSetup.toggle_getflt = FALSE;
  }

  /* pre-load AER tail model filter */
  if (siuSetup.toggle_putflt) {
    if(siuSetup.aer_kernel_srate == AER_SIM_SRATE_16000_DIV_8K) {
      num_coeff_words = aer_NUM_WORDS_PER_H_VEC_16K*NUM_H_VEC_PUT;
    }
    else {
      num_coeff_words = aer_NUM_WORDS_PER_H_VEC_8K*NUM_H_VEC_PUT;
    }

    /* load valid tail model through CCS before executing code below */
    ret_code = aerPutFilter(inst->aerHFInst[0], &aer_tail_model, &aer_coef_mant[0],
                 &aer_coef_exp[0], 0, aer_NUM_WORDS_PER_H_VEC_16K, FALSE);
    if(ret_code != aer_NOERR) {
      //printf("Error when calling aerPutFilter with error code %d!\n", ret_code);
      exit(0);
    }
    ret_code = aerPutFilter(inst->aerHFInst[0], &aer_tail_model,
                            &aer_coef_mant[aer_NUM_WORDS_PER_H_VEC_16K],
                            &aer_coef_exp[0], aer_NUM_WORDS_PER_H_VEC_16K,
                            aer_NUM_WORDS_PER_H_VEC_16K, FALSE);
    if(ret_code != aer_NOERR) {
      //printf("Error when calling aerPutFilter with error code %d!\n", ret_code);
      exit(0);
    }
    ret_code = aerPutFilter(inst->aerHFInst[0], &aer_tail_model,
                            &aer_coef_mant[aer_NUM_WORDS_PER_H_VEC_16K*2],
                            &aer_coef_exp[0], aer_NUM_WORDS_PER_H_VEC_16K*2,
                            aer_NUM_WORDS_PER_H_VEC_16K, TRUE);
    if(ret_code != aer_NOERR) {
      //printf("Error when calling aerPutFilter with error code %d!\n", ret_code);
      exit(0);
    }

    siuSetup.toggle_putflt = FALSE;
  }

/* code below can be used to test adaptive AGC
  if(frm_cnt == 1000) {
    siuSetup.agcCtl.valid_bitfield = agc_CTL_VALID_SAT_THRESHOLD;
    siuSetup.agcCtl.sat_threshold  = 1024;
    agcControl (inst->agcHFInst[0], (agcControl_t *)&siuSetup.agcCtl);

    printf("Start filter rescaling test. Reduce AGC saturation threshold.\n");
  }

  if(frm_cnt == 2000) {
    siuSetup.agcCtl.valid_bitfield = agc_CTL_VALID_SAT_THRESHOLD;
    siuSetup.agcCtl.sat_threshold  = 32500;
    agcControl (inst->agcHFInst[0], (agcControl_t *)&siuSetup.agcCtl);
    printf("Change AGC saturation threshold back to what it was.\n");
  }
*/
} /* aer_sim_cfg_on_the_fly */


/******************************************************************************
 * FUNCTION PURPOSE: Print AER version number and measured MIPS.
 *****************************************************************************/
void aer_sim_print_version_mips(siuInst_t *inst)
{
  aerDebugStat_t aer_dbg;
  aerVersion_t aer_ver;

  aerGetPerformance(inst->aerHFInst[0], &aer_dbg, &aer_ver, FALSE);

  //printf("AER version: %d.%d.%d.%d.%d.%d\n", aer_ver.major, aer_ver.minor,
  //        aer_ver.patch, aer_ver.build, aer_ver.quality, aer_ver.btype);

  if(siuSetup.aer_mips_profile) {
#ifdef ti_targets_C55_large
    //printf("C55x: AER Tx Max Cycles = %ld, Avg Cycles = %ld\n",
    //       siuSetup.TxCyclesMax, siuSetup.TxCyclesAvg);
    //printf("C55x: AER Rx Max Cycles = %ld, Avg Cycles = %ld\n",
    //       siuSetup.RxCyclesMax, siuSetup.RxCyclesAvg);
#else
#ifndef gnu_targets_arm_GCArmv7A/* c64x+ */
    printf("C64x+/C674x: AER Tx Max Cycles = %d, Avg Cycles = %d\n",
           siuSetup.TxCyclesMax, siuSetup.TxCyclesAvg);
    printf("C64x+/C674x: AER Rx Max Cycles = %d, Avg Cycles = %d\n",
           siuSetup.RxCyclesMax, siuSetup.RxCyclesAvg);
#endif
#endif

    //printf("MIPS measurement done\n");
  }
} /* aer_sim_print_version_mips */

CSL_IRQ_Dispatch     dispatchTable;



///////////////////////////////////////////////////////////////////////////////
/* -------------------- MAIN SIMULATION FUNCTION --------------------------- */
/////////////////////////////////////////////////////////////////////////////

int main()
{
    tint num_mic, mic_type;

    DeviceInit();
    DeviceStart();

    aer_sim_init(&siuSetup);
    aer_sim_get_cfg(&siuSetup);

    mic_type = siuSetup.system_cfg.mult_mic_type;
    if(mic_type == AER_SIM_MIC_TYPE_ARRAY) {
      num_mic = siuSetup.system_cfg.num_BF_mic;
    }
    else {
      num_mic = siuSetup.system_cfg.num_HF_mic;
    }

    aer_sim_apply_config(&siuSetup);
    aer_sim_init_siu(&siu_inst, &siuSetup);
    aer_sim_init_piu(&piu_inst, &siuSetup);
    aer_sim_instantiate_aer(&siu_inst, &siuSetup);
    aer_sim_open_aep(&aepSimInst, &siuSetup);
    aer_sim_config_aer_params(&siu_inst, &siuSetup);
    aer_sim_aep_config(&aepSimInst, &siuSetup.aep_params,
                       siuSetup.aep_gain_adj_exp, siuSetup.aep_gain_adj_mant);


    //aerControl_t aer_ctl;

    //***** LOOP ****
    loop {
      if(flagUART_RX){
          flagUART_RX = 0;
          UART_params_apply();
      }

      aer_sim_cfg_on_the_fly(&siu_inst);

      frm_cnt++;
      if(frm_cnt ==50000)
          GPIO_write(hGpio17, CSL_GPIO_PIN14, 1);
      if(frm_cnt ==100000){
                GPIO_write(hGpio17, CSL_GPIO_PIN14, 0);
                frm_cnt = 0;
      }

      if(F_read_block(fr_bf))
      {
          if(TRUE)//aer_off_music == 0)
          {
              siuReceiveIn(&siu_inst, fr_bf, sim_data_rx_out, NULL,
                           siuSetup.system_cfg.num_HF_mic);
              piuReceiveIn(&piu_inst, sim_data_rx_out, sim_data_dac, sim_data_rx_sync);
          }

          switch(spkr_sel)
          {
              case 0:
                  spkr_writeL_block(bf_null[0]);
                  //spkr_writeR_block(bf_null[0]);
                  break;
              case 1:
                  if(aer_off_music)
                      spkr_writeL_block(fr_bf);
                  else
                      spkr_writeL_block(sim_data_dac);
                  break;
              case 2:
                  /*if(aer_off_music)
                      spkr_writeL_block(fr_bf);
                  else
                  spkr_writeR_block(sim_data_dac);*/
                  break;
          }
      }

      switch(mic_sel)
      {
          case 0:
              if(mic_readL_block(sim_data_ne_speech[0]))
              {
                  //��� ��������� ���������, ������ ������� �����
                  aer_sim_aep_add_echo(&aepSimInst, sim_data_dac, bf_null,
                                           sim_data_mic, num_mic, 1);
                  piuSendIn(&piu_inst, sim_data_mic, sim_data_tx_in, num_mic);
                  siuSendIn(&siu_inst, sim_data_rx_sync, sim_data_tx_in, sim_data_tx_out,
                                NULL, num_mic, mic_type, siuSetup.aer_sout_frm_size);
                  F_write_block(sim_data_tx_out);
              }
              break;
          case 1:
              if(mic_readR_block(sim_data_ne_speech[0]))
              {
                  //�������� ��������_1 (����� ����� I2S)
                  aer_sim_aep_add_echo(&aepSimInst, sim_data_dac, sim_data_ne_speech,
                                       sim_data_mic, num_mic, 1);
                  piuSendIn(&piu_inst, sim_data_mic, sim_data_tx_in, num_mic);
                  siuSendIn(&siu_inst, sim_data_rx_sync, sim_data_tx_in, sim_data_tx_out,
                            NULL, num_mic, mic_type, siuSetup.aer_sout_frm_size);
                  F_write_block(sim_data_tx_out);
              }
              break;
          case 2:
              if(mic_readL_block(sim_data_ne_speech[0]))
              {
                  //�������� ��������_2 (������ ����� I2S)
                  aer_sim_aep_add_echo(&aepSimInst, sim_data_dac, sim_data_ne_speech,
                                       sim_data_mic, num_mic, 1);
                  piuSendIn(&piu_inst, sim_data_mic, sim_data_tx_in, num_mic);
                  siuSendIn(&siu_inst, sim_data_rx_sync, sim_data_tx_in, sim_data_tx_out,
                            NULL, num_mic, mic_type, siuSetup.aer_sout_frm_size);
                  F_write_block(sim_data_tx_out);
              }
              break;
      }


    }
    return(0);
}

//*****************************************************************************
// DeviceInit
//*****************************************************************************
void DeviceInit()
{
    PLL_Obj                 pllObj;
    PLL_Config              *configInfo;
    PLL_Handle              hPll;
    Uint32                  pllInstId;
    int i;
    Uint16 prcr;

   CSL_SYSCTRL_REGS->PCGCR1 = 0x0000;
   CSL_SYSCTRL_REGS->PCGCR2 = 0x0000;

   IRQ_init(&dispatchTable, 0);
   IRQ_globalDisable();
   IRQ_disableAll();
   IRQ_clearAll();

   IRQ_setVecs((Uint32)&VECSTART);

   // Set PLL
   const PLL_Config pllCfg_100MHz      = {0x8C31, 0x0173, 0x0806, 0x0000}; //from 12MHz
   pllInstId = 0;
   PLL_init(&pllObj,pllInstId);
   hPll = &pllObj;
   PLL_reset(hPll);
   configInfo = (PLL_Config *)&pllCfg_100MHz;
   PLL_config(hPll, configInfo);
   for(i=0;i<100;i++);
   PLL_enable(hPll);
   for(i=0;i<100;i++);

   //Set PinMap
   CSL_FINST(CSL_SYSCTRL_REGS->EBSR, SYS_EBSR_PPMODE, MODE1);
   CSL_FINST(CSL_SYSCTRL_REGS->EBSR, SYS_EBSR_SP1MODE, MODE0);
   CSL_FINST(CSL_SYSCTRL_REGS->EBSR, SYS_EBSR_SP0MODE, MODE1);

   // Enable HWA, CPU, DPORT, MPORT, XPORT, and IPORT in ICR */
   *(volatile ioport Uint16 *)(0x0001) = 0x000E;
   /* Execute idle instruction */
   asm(" idle");

   //Enable peripherals
   CSL_SYSCTRL_REGS->PCGCR1 = 0x1c02;
   CSL_SYSCTRL_REGS->PCGCR2 = 0x0003;

   // Reset all peripherals
   CSL_SYSCTRL_REGS->PSRCR = 0x0020;
   CSL_SYSCTRL_REGS->PRCR = 0x00BB;
   do
   {
       prcr = CSL_SYSCTRL_REGS->PRCR;
   } while (prcr != 0);
}
//---------------------------------------------------------------

void DeviceStart()
{
    int i, a;
    for(i=0; i<FRAME_LENGTH*2; i++){
        bufN_WL[i] = 0;
        bufN_WR[i] = 0;
        bufN_RL[i] = 0;
        bufN_RR[i] = 0;
        bufF_W[i] = 0;
        bufF_R[i] = 0;
    }
    for(a=0; a<AER_SIM_NUM_MIC; a++)
        for(i=0; i<SIU_AER_MAX_FRAME_LENGTH; i++)
            bf_null[a][i] = 0x0;
    for(i=0; i<100; i++)
        bufUART[i] = 0;

    GPIO_init();
    GPIO_write(hGpio17, CSL_GPIO_PIN17, 1);// ����� AIC
    Wait(100000);
    
    i2c_init();
    Wait(300);
    UARTinit();
    DmaInit();
    I2sDmaF_init();
    I2sDmaN_init();
    i2sF_init();
    i2sN_init();
    aic_init();
    IRQ_globalEnable();
}

//****************************************************************************
// GPIO_init();
//****************************************************************************
void GPIO_init()
{
    CSL_Status           status;
    CSL_GpioPinConfig    config;

      // Make Serial port 0 and 1, parallel port's 8 pin and
      // A15 to A20 pin as GPIO
      //
    //CSL_FINST(CSL_SYSCTRL_REGS->EBSR, SYS_EBSR_SP0MODE, MODE2);

     // Open GPIO module
    //hGpio12 = GPIO_open(&gpioObj12, &status);
    //hGpio13 = GPIO_open(&gpioObj13, &status);
    hGpio14 = GPIO_open(&gpioObj14, &status);
    //hGpio16 = GPIO_open(&gpioObj16, &status);
    hGpio17 = GPIO_open(&gpioObj17, &status);

     // Configure GPIO
/*    config.pinNum    = CSL_GPIO_PIN12;
    config.direction = CSL_GPIO_DIR_OUTPUT;
    config.trigger   = CSL_GPIO_TRIG_CLEAR_EDGE;
    GPIO_configBit(hGpio12, &config);

    config.pinNum    = CSL_GPIO_PIN13;
    config.direction = CSL_GPIO_DIR_OUTPUT;
    config.trigger   = CSL_GPIO_TRIG_CLEAR_EDGE;
    GPIO_configBit(hGpio13, &config);
*/
    config.pinNum    = CSL_GPIO_PIN14;
    config.direction = CSL_GPIO_DIR_OUTPUT;
    config.trigger   = CSL_GPIO_TRIG_CLEAR_EDGE;
    GPIO_configBit(hGpio14, &config);

/*    config.pinNum    = CSL_GPIO_PIN16;
    config.direction = CSL_GPIO_DIR_OUTPUT;
    config.trigger   = CSL_GPIO_TRIG_CLEAR_EDGE;
    GPIO_configBit(hGpio16, &config);
*/
    config.pinNum    = CSL_GPIO_PIN17;
    config.direction = CSL_GPIO_DIR_OUTPUT;
    config.trigger   = CSL_GPIO_TRIG_CLEAR_EDGE;
    GPIO_configBit(hGpio17, &config);

    int i;
     // Write 1 to output pin

//    GPIO_write(hGpio12, CSL_GPIO_PIN12, 1);
//    GPIO_write(hGpio13, CSL_GPIO_PIN13, 1);
//    GPIO_write(hGpio14, CSL_GPIO_PIN14, 1);
//    GPIO_write(hGpio16, CSL_GPIO_PIN16, 1);*/
    GPIO_write(hGpio17, CSL_GPIO_PIN17, 1);

    Wait(10000);
//    GPIO_write(hGpio12, CSL_GPIO_PIN12, 0);
//    GPIO_write(hGpio13, CSL_GPIO_PIN13, 0);
//    GPIO_write(hGpio14, CSL_GPIO_PIN14, 0);
//    GPIO_write(hGpio16, CSL_GPIO_PIN16, 0);*/
    GPIO_write(hGpio17, CSL_GPIO_PIN17, 0);
    Wait(10000);
}

//*****************************************************************************
// DmaInit
//  Description: Initializes DMA, enables DMA interrupts
//*****************************************************************************
void DmaInit()
{
    Uint16 ifrValue;

    IRQ_disable(DMA_EVENT);
    IRQ_clear(DMA_EVENT);
    CSL_SYSCTRL_REGS->DMAIER = 0x0000;// Disable DMA interrupts
    ifrValue = CSL_SYSCTRL_REGS->DMAIFR;// Clear pending DMA interrupts
    CSL_SYSCTRL_REGS->DMAIFR |= ifrValue;
    IRQ_plug(DMA_EVENT, &DmaIsr);
    IRQ_enable(DMA_EVENT);
    DMA_init();
}
//-----------------------------------------------------------------------------

//*****************************************************************************
//  void i2s_init()
//****************************************************************************
void i2sN_init()
{
    CSL_I2sHandle hI2sN;
    I2S_Config      hwConfig;

    // Open the device with instance 2
    hI2sN = I2S_open(I2S_INSTANCE2, DMA_INTERRUPT, I2S_CHAN_STEREO);

    // Set the value for the configure structure
    hwConfig.dataType           = I2S_STEREO_ENABLE;
    hwConfig.loopBackMode       = I2S_LOOPBACK_DISABLE;
    hwConfig.fsPol              = I2S_FSPOL_LOW;
    hwConfig.clkPol             = I2S_RISING_EDGE;
    hwConfig.datadelay          = I2S_DATADELAY_ONEBIT;
    hwConfig.datapack           = I2S_DATAPACK_ENABLE;
    hwConfig.signext            = I2S_SIGNEXT_DISABLE;
    hwConfig.wordLen            = I2S_WORDLEN_16;
    hwConfig.i2sMode            = I2S_SLAVE;
    hwConfig.FError             = I2S_FSERROR_DISABLE;
    hwConfig.OuError            = I2S_OUERROR_DISABLE;
    hwConfig.clkDiv             = I2S_CLKDIV128;
    hwConfig.dataFormat         = I2S_DATAFORMAT_DSP;
    hwConfig.fsDiv              = I2S_FSDIV32;

    // Configure hardware registers
    I2S_setup(hI2sN, &hwConfig);
    I2S_transEnable(hI2sN, TRUE);
    hI2sN->firstRead = FALSE;
}
//-----------------------------------------------------------------------------

void i2sF_init()
{
    CSL_I2sHandle hI2sF;
    I2S_Config      hwConfig;

    /* Open the device with instance 2 */
    hI2sF = I2S_open(I2S_INSTANCE0, DMA_INTERRUPT, I2S_CHAN_STEREO);

    /* Set the value for the configure structure */
    hwConfig.dataType           = I2S_STEREO_ENABLE;
    hwConfig.loopBackMode       = I2S_LOOPBACK_DISABLE;
    hwConfig.fsPol              = I2S_FSPOL_LOW;
    hwConfig.clkPol             = I2S_RISING_EDGE;
    hwConfig.datadelay          = I2S_DATADELAY_ONEBIT;
    hwConfig.datapack           = I2S_DATAPACK_ENABLE;
    hwConfig.signext            = I2S_SIGNEXT_DISABLE;
    hwConfig.wordLen            = I2S_WORDLEN_16;
    hwConfig.i2sMode            = I2S_SLAVE;
    hwConfig.FError             = I2S_FSERROR_ENABLE;
    hwConfig.OuError            = I2S_OUERROR_ENABLE;
    hwConfig.clkDiv             = I2S_CLKDIV16;
    hwConfig.dataFormat         = I2S_DATAFORMAT_DSP;
    hwConfig.fsDiv              = I2S_FSDIV16;

    /* Configure hardware registers */
    I2S_setup(hI2sF, &hwConfig);
    I2S_transEnable(hI2sF, TRUE);
    hI2sF->firstRead = FALSE;
}


//*****************************************************************************
// I2sDmaInit
// Configures and starts I2S with DMA
//*****************************************************************************
void I2sDmaN_init()
{
    CSL_DMA_Config dmaConfig;
    CSL_Status status;


    // Configure DMA ch4 for I2S write left
    dmaConfig.pingPongMode  = CSL_DMA_PING_PONG_ENABLE;
    dmaConfig.autoMode      = CSL_DMA_AUTORELOAD_ENABLE;
    dmaConfig.burstLen      = CSL_DMA_TXBURST_1WORD;
    dmaConfig.trigger       = CSL_DMA_EVENT_TRIGGER;
    dmaConfig.dmaEvt        = CSL_DMA_EVT_I2S2_TX;
    dmaConfig.dmaInt        = CSL_DMA_INTERRUPT_ENABLE;
    dmaConfig.chanDir       = CSL_DMA_WRITE;
    dmaConfig.trfType       = CSL_DMA_TRANSFER_IO_MEMORY;
    dmaConfig.dataLen       = FRAME_LENGTH*4; // two frames
    dmaConfig.srcAddr       = (Uint32)bufN_WLPi;
    dmaConfig.destAddr      = (Uint32)&CSL_I2S2_REGS->I2STXLT0;

    dmaNLTxHandle = DMA_open(DMA_NL_CHAN_TX, &dmaObj0,&status);
    status = DMA_config(dmaNLTxHandle, &dmaConfig);
    DMA_start (dmaNLTxHandle);

/*    // Configure DMA ch5 for I2S write right
    dmaConfig.pingPongMode  = CSL_DMA_PING_PONG_ENABLE;
    dmaConfig.autoMode      = CSL_DMA_AUTORELOAD_ENABLE;
    dmaConfig.burstLen      = CSL_DMA_TXBURST_1WORD;
    dmaConfig.trigger       = CSL_DMA_EVENT_TRIGGER;
    dmaConfig.dmaEvt        = CSL_DMA_EVT_I2S2_TX;
    dmaConfig.dmaInt        = CSL_DMA_INTERRUPT_ENABLE;
    dmaConfig.chanDir       = CSL_DMA_WRITE;
    dmaConfig.trfType       = CSL_DMA_TRANSFER_IO_MEMORY;
    dmaConfig.dataLen       = FRAME_LENGTH*4; // two frames
    dmaConfig.srcAddr       = (Uint32)bufN_WRPi;
    dmaConfig.destAddr      = (Uint32)&CSL_I2S2_REGS->I2STXRT0;

    dmaNRTxHandle = DMA_open(DMA_NR_CHAN_TX, &dmaObj4,&status);
    status = DMA_config(dmaNRTxHandle, &dmaConfig);
    DMA_start (dmaNRTxHandle);
*/
    // Configure DMA ch6 for I2S left read
    dmaConfig.pingPongMode  = CSL_DMA_PING_PONG_ENABLE;
    dmaConfig.autoMode      = CSL_DMA_AUTORELOAD_ENABLE;
    dmaConfig.burstLen      = CSL_DMA_TXBURST_1WORD;
    dmaConfig.trigger       = CSL_DMA_EVENT_TRIGGER;
    dmaConfig.dmaEvt        = CSL_DMA_EVT_I2S2_RX;
    dmaConfig.dmaInt        = CSL_DMA_INTERRUPT_ENABLE;
    dmaConfig.chanDir       = CSL_DMA_READ;
    dmaConfig.trfType       = CSL_DMA_TRANSFER_IO_MEMORY;
    dmaConfig.dataLen       = FRAME_LENGTH*4; // two frames
    dmaConfig.srcAddr       = (Uint32)&CSL_I2S2_REGS->I2SRXLT0;
    dmaConfig.destAddr      = (Uint32)bufN_RLPi;

    dmaNLRxHandle = DMA_open(DMA_NL_CHAN_RX, &dmaObj1,&status);
    DMA_config(dmaNLRxHandle, &dmaConfig);
    DMA_start (dmaNLRxHandle);

   // Configure DMA ch7 for I2S right read
    dmaConfig.pingPongMode  = CSL_DMA_PING_PONG_ENABLE;
    dmaConfig.autoMode      = CSL_DMA_AUTORELOAD_ENABLE;
    dmaConfig.burstLen      = CSL_DMA_TXBURST_1WORD;
    dmaConfig.trigger       = CSL_DMA_EVENT_TRIGGER;
    dmaConfig.dmaEvt        = CSL_DMA_EVT_I2S2_RX;
    dmaConfig.dmaInt        = CSL_DMA_INTERRUPT_ENABLE;
    dmaConfig.chanDir       = CSL_DMA_READ;
    dmaConfig.trfType       = CSL_DMA_TRANSFER_IO_MEMORY;
    dmaConfig.dataLen       = FRAME_LENGTH*4; // two frames
    dmaConfig.srcAddr       = (Uint32)&CSL_I2S2_REGS->I2SRXRT0;
    dmaConfig.destAddr      = (Uint32)bufN_RRPi;

    dmaNRRxHandle = DMA_open(DMA_NR_CHAN_RX, &dmaObj5,&status);
    DMA_config(dmaNRRxHandle, &dmaConfig);
    DMA_start (dmaNRRxHandle);

    flagN_RLI = 0;
    flagN_RRI = 0;
    flagN_WLI = 0;
    flagN_WRI = 0;
}
//------------------------------------------------------------------

void I2sDmaF_init()
{
    CSL_DMA_Config dmaConfig;
    CSL_Status status;


    // Configure DMA ch0 for I2S write
    dmaConfig.pingPongMode  = CSL_DMA_PING_PONG_ENABLE;
    dmaConfig.autoMode      = CSL_DMA_AUTORELOAD_ENABLE;
    dmaConfig.burstLen      = CSL_DMA_TXBURST_1WORD;
    dmaConfig.trigger       = CSL_DMA_EVENT_TRIGGER;
    dmaConfig.dmaEvt        = CSL_DMA_EVT_I2S0_TX;
    dmaConfig.dmaInt        = CSL_DMA_INTERRUPT_ENABLE;
    dmaConfig.chanDir       = CSL_DMA_WRITE;
    dmaConfig.trfType       = CSL_DMA_TRANSFER_IO_MEMORY;
    dmaConfig.dataLen       = FRAME_LENGTH*4; // two frames
    dmaConfig.srcAddr       = (Uint32)bufF_WPi;
    dmaConfig.destAddr      = (Uint32)&CSL_I2S0_REGS->I2STXLT0;

    dmaFTxHandle = DMA_open(DMA_F_CHAN_TX, &dmaObj2,&status);
    status = DMA_config(dmaFTxHandle, &dmaConfig);
    DMA_start (dmaFTxHandle);

    // Configure DMA ch2 for I2S read
    dmaConfig.pingPongMode  = CSL_DMA_PING_PONG_ENABLE;
    dmaConfig.autoMode      = CSL_DMA_AUTORELOAD_ENABLE;
    dmaConfig.burstLen      = CSL_DMA_TXBURST_1WORD;
    dmaConfig.trigger       = CSL_DMA_EVENT_TRIGGER;
    dmaConfig.dmaEvt        = CSL_DMA_EVT_I2S0_RX;
    dmaConfig.dmaInt        = CSL_DMA_INTERRUPT_ENABLE;
    dmaConfig.chanDir       = CSL_DMA_READ;
    dmaConfig.trfType       = CSL_DMA_TRANSFER_IO_MEMORY;
    dmaConfig.dataLen       = FRAME_LENGTH*4; // two frames
    dmaConfig.srcAddr       = (Uint32)&CSL_I2S0_REGS->I2SRXLT0;
    dmaConfig.destAddr      = (Uint32)bufF_RPi;

    dmaFRxHandle = DMA_open(DMA_F_CHAN_RX, &dmaObj3,&status);
    DMA_config(dmaFRxHandle, &dmaConfig);
    DMA_start (dmaFRxHandle);

    flagF_RI = 0;
    flagF_WI = 0;
}
//------------------------------------------------------------------

//*****************************************************************
// Iterupt DMA
//*****************************************************************

interrupt void DmaIsr(void)
{
    CSL_Status status;
    volatile Uint16 ifrValue;
    Uint16 gp;

    // Clear the DMA interrupt
    ifrValue = CSL_SYSCTRL_REGS->DMAIFR;
    CSL_SYSCTRL_REGS->DMAIFR |= ifrValue;

    //Ch 0 Write to ������� �����
    if (ifrValue & (1<<0)){
        flagF_WI = 1;
        if(DMA_getLastTransferType (dmaFTxHandle, &status)){
            flagF_WPP = 0;
        }
        else{
            flagF_WPP = 1;
        }
    }

    //Ch 2 Read from ������� �����
    if (ifrValue & (1<<2)){
        flagF_RI = 1;
        if(DMA_getLastTransferType (dmaFRxHandle, &status)){
            flagF_RPP = 0;
        }
        else{
            flagF_RPP = 1;
        }
    }

    //Ch 4 Write to left SPKR
    if (ifrValue & (1<<4)){
        flagN_WLI = 1;
        if(DMA_getLastTransferType (dmaNLTxHandle, &status)){
            flagN_WLPP = 0;
        }
        else{
            flagN_WLPP = 1;
        }
    }

/*    //Ch 5 Write to right SPKR
    if (ifrValue & (1<<5)){
        flagN_WRI = 1;
        if(DMA_getLastTransferType (dmaNRTxHandle, &status)){
            flagN_WRPP = 0;
        }
        else{
            flagN_WRPP = 1;
        }
    }
*/
    //Ch 6 Read from left MIC
    if (ifrValue & (1<<6)){
        flagN_RLI = 1;
        if(DMA_getLastTransferType (dmaNLRxHandle, &status)){
            flagN_RLPP = 0;
        }
        else{
            flagN_RLPP = 1;
        }
    }

    //Ch 7 Read from right MIC
    if (ifrValue & (1<<6)){
        flagN_RRI = 1;
        if(DMA_getLastTransferType (dmaNRRxHandle, &status)){
            flagN_RRPP = 0;
        }
        else{
            flagN_RRPP = 1;
        }
    }
}
//-------------------------------------------------------------------------------

Bool mic_readL_block(int* buffer)
{
    int i;
    Uint32* bL = (Uint32*)buffer;
    Uint32* dma;

    if(flagN_RLI)
        flagN_RLI = 0;
    else
        return FALSE;
    if(flagN_RLPP == 1){
        dma = (Uint32*)(&bufN_RL[0]);
        for (i = 0; i < FRAME_LENGTH/2; i++)
            *bL++ = *dma++;
    }
    else{
        dma = (Uint32*)(&bufN_RL[FRAME_LENGTH]);
        for (i = 0; i < FRAME_LENGTH/2; i++)
            *bL++ = *dma++;
    }
    return TRUE;
}
//------------------------------------------------------------------

Bool mic_readR_block(int* buffer)
{
    int i;
    Uint32* bL = (Uint32*)buffer;
    Uint32* dma;

    if(flagN_RRI)
        flagN_RRI = 0;
    else
        return FALSE;
    if(flagN_RRPP == 1){
        dma = (Uint32*)(&bufN_RR[0]);
        for (i = 0; i < FRAME_LENGTH/2; i++)
            *bL++ = *dma++;
    }
    else{
        dma = (Uint32*)(&bufN_RR[FRAME_LENGTH]);
        for (i = 0; i < FRAME_LENGTH/2; i++)
            *bL++ = *dma++;
    }
    return TRUE;
}
//------------------------------------------------------------------

Bool spkr_writeL_block(int* buffer)
{
    int i;
    Uint32* bL = (Uint32*)buffer;
    Uint32* dma;

    //while(flagN_WI == 0);
    //flagN_WI = 0;
    if(flagN_WLI)
        flagN_WLI = 0;
    else
        return FALSE;
    if(flagN_WLPP == 1){
        dma = (Uint32*)(&bufN_WL[0]);
        for (i = 0; i < FRAME_LENGTH/2; i++)
            *dma++ = *bL++;
    }
    else {
        dma = (Uint32*)(&bufN_WL[FRAME_LENGTH]);
        for (i = 0; i < FRAME_LENGTH/2; i++)
            *dma++ = *bL++;
    }
    return TRUE;
}
//-------------------------------------------------------------------------

Bool spkr_writeR_block(int* buffer)
{
    int i;
    Uint32* bL = (Uint32*)buffer;
    Uint32* dma;

    //while(flagN_WI == 0);
    //flagN_WI = 0;
    if(flagN_WRI)
        flagN_WRI = 0;
    else
        return FALSE;
    if(flagN_WRPP == 1){
        dma = (Uint32*)(&bufN_WR[0]);
        for (i = 0; i < FRAME_LENGTH/2; i++)
            *dma++ = *bL++;
    }
    else {
        dma = (Uint32*)(&bufN_WR[FRAME_LENGTH]);
        for (i = 0; i < FRAME_LENGTH/2; i++)
            *dma++ = *bL++;
    }
    return TRUE;
}
//-------------------------------------------------------------------------

Bool F_read_block(int* buffer)
{
    int i;
    Uint32* bL = (Uint32*)buffer;
    Uint32* dma;

    //while(flagF_RI == 0);
    //flagF_RI = 0;
    if(flagF_RI)
        flagF_RI = 0;
    else
        return FALSE;
    if(flagF_RPP == 1){
        dma = (Uint32*)(&bufF_R[0]);
        for (i = 0; i < FRAME_LENGTH/2; i++)
            *bL++ = *dma++;
    }
    else{
        dma = (Uint32*)(&bufF_R[FRAME_LENGTH]);
        for (i = 0; i < FRAME_LENGTH/2; i++)
            *bL++ = *dma++;
    }
    return TRUE;
}
//------------------------------------------------------------------

Bool F_write_block(int* buffer)
{
    int i;
    Uint32* bL = (Uint32*)buffer;
    Uint32* dma;

    //while(flagF_WI == 0);
    //flagF_WI = 0;
    if(flagF_WI)
        flagF_WI = 0;
    else
        return FALSE;
    if(flagF_WPP == 1){
        dma = (Uint32*)(&bufF_W[0]);
        for (i = 0; i < FRAME_LENGTH/2; i++)
            *dma++ = *bL++;
    }
    else {
        dma = (Uint32*)(&bufF_W[FRAME_LENGTH]);
        for (i = 0; i < FRAME_LENGTH/2; i++)
            *dma++ = *bL++;
    }
    return TRUE;
}
//-------------------------------------------------------------------------

//*************************************************************************
//I2C Init
//*************************************************************************
void i2c_init()
{
    volatile Uint16    looper;
    volatile Uint32    csl_i2c_sys_clk;


    // Initialize I2C module
    I2C_init(CSL_I2C0);

    csl_i2c_sys_clk = GetSysClk()/1000;
    // Setup I2C module
    i2cSetup.addrMode    = CSL_I2C_ADDR_7BIT;
    i2cSetup.bitCount    = CSL_I2C_BC_8BITS;
    i2cSetup.loopBack    = CSL_I2C_LOOPBACK_DISABLE;
    i2cSetup.freeMode    = CSL_I2C_FREEMODE_DISABLE;
    i2cSetup.repeatMode  = CSL_I2C_REPEATMODE_DISABLE;
    i2cSetup.ownAddr     = CSL_I2C_OWN_ADDR;
    //sysclk to i2c, before pre-scaling
    i2cSetup.sysInputClk = csl_i2c_sys_clk/1000u;
    //actual i2c serial clk
    i2cSetup.i2cBusFreq = CSL_I2C_BUS_FREQ;
    startStop            = ((CSL_I2C_START) | (CSL_I2C_STOP));

    I2C_setup(&i2cSetup);
}
//-----------------------------------------------------------------

Uint32 GetSysClk()
{
    Bool      pllRDBypass;
    Bool      pllOutDiv;
    Uint32    sysClk;
    Uint16    pllM;
    Uint16    pllRD;
    Uint16    pllOD;

    pllM = CSL_FEXT(CSL_SYSCTRL_REGS->CGCR1, SYS_CGCR1_M);

    pllRD = CSL_FEXT(CSL_SYSCTRL_REGS->CGCR2, SYS_CGCR2_RDRATIO);
    pllOD = CSL_FEXT(CSL_SYSCTRL_REGS->CGCR4, SYS_CGCR4_ODRATIO);

    pllRDBypass = CSL_FEXT(CSL_SYSCTRL_REGS->CGCR2, SYS_CGCR2_RDBYPASS);
    pllOutDiv   = CSL_FEXT(CSL_SYSCTRL_REGS->CGCR4, SYS_CGCR4_OUTDIVEN);

    sysClk = 12000000u;//12MHz

    if (0 == pllRDBypass)
    {
        sysClk = sysClk/(pllRD + 4);
    }

    sysClk = (sysClk * (pllM + 4));

    if (1 == pllOutDiv)
    {
        sysClk = sysClk/(pllOD + 1);
    }

    // Return the value of system clock in KHz
    return(sysClk);
}
//-------------------------------------------------------------------------

//*************************************************************************
// AIC Init
//************************************************************************
Int16 AIC3204_rget(  Uint16 regnum, Uint16* regval )
{
    Uint16 val[1];

    regnum = (regnum & 0x00FF);

    Uint16 startStop = ((CSL_I2C_START) | (CSL_I2C_STOP));
    I2C_read(val, 1, AIC3204_I2C_ADDR, &regnum, 1, TRUE, startStop,
                 CSL_I2C_MAX_TIMEOUT, FALSE);

    Wait(1000);
    *regval = val[0];
    return val[0];
}
//--------------------------------------------------------------------------

void AIC3204_rset( Uint16 regnum, Uint16 regval )
{
    Uint16 cmd[2];
    cmd[0] = (regnum & 0x00FF);       // 7-bit Device Register
    cmd[1] = (regval & 0x00FF);                // 8-bit Register Data

   Uint16 startStop = ((CSL_I2C_START) | (CSL_I2C_STOP));
   I2C_write(cmd, 2, AIC3204_I2C_ADDR, TRUE, startStop,
                       CSL_I2C_MAX_TIMEOUT);
   Wait(1000);
}


//****************************************************************************
//AIC init
//****************************************************************************
void aic_init()
{
    Uint16 regval = 0;

    // Configure AIC3204
    AIC3204_rset( 0,  0x00 );  // Select page 0

    AIC3204_rset( 1,  0x01 );  // Reset codec
    Wait(1000);  // Wait 1ms after reset
    AIC3204_rset( 0,  0x01 );  // Select page 1
    AIC3204_rset( 1,  0x08 );  // Disable crude AVDD generation from DVDD
    AIC3204_rset( 2,  0x01 );  // Enable Analog Blocks, use LDO power
    AIC3204_rset( 123,0x05 );  // Force reference to power up in 40ms
    Wait(50000); // Wait at least 40ms
    AIC3204_rset( 0,  0x00 );  // Select page 0

    // PLL and Clocks config and Power Up
    if(AIC_SAMPLE_SIZE == 32)
        AIC3204_rset( 27, 0x3d );  // BCLK and WCLK are set as o/p; AIC3204(Master); 32-bit sample
    else
        AIC3204_rset( 27, 0x0d );  // BCLK and WCLK are set as o/p; AIC3204(Master); 16-bit sample
    AIC3204_rget(27, &regval);
    AIC3204_rset( 28, 0x00 );  // Data ofset = 0
	
	//Reg.4 �������� 3 - clock ������ ������� (MCLK=12���), �� ���� �������� PLLCLK ���������� �� PLL. For MASTER
    AIC3204_rset( 4,  0x03 );  // PLL setting: PLLCLK <- MCLK, CODEC_CLKIN <-PLL CLK.
    AIC3204_rget(4, &regval);
    //Reg.4 �������� 7 - clock ������� �� I2S (BCLK=32���), �� ���� �������� PLLCLK ��������� �� PLL. For SLAVE
    //AIC3204_rset( 4,  0x07 );  // PLL setting: PLLCLK <- BCLK, CODEC_CLKIN <-PLL CLK.
    
	//������������� PLL = 7,168. ����� ������� ������� CODEC_CLK = BCLK*PLL = 1,024��� * 48 * 2 = 98.304.000  For SLAVE
	/*AIC3204_rset( 5,  0x92 );  // PLL setting: Power up PLL, P=1 and R=2
    AIC3204_rset( 6,  0x30 );  // PLL setting: J=48
    AIC3204_rset( 7,  0x00 );  // PLL setting: HI_BYTE(D=0)
    AIC3204_rset( 8,  0x00 );  // PLL setting: LO_BYTE(D=0)*/
    
	AIC3204_rset( 30, 0x88 );  // For 32 bit clocks per frame in Master mode ONLY
                               // BCLK=DAC_CLK/N =(12288000/8) = 1.536MHz = 32*fs
    Wait(10000); // Wait for PLL to come up
    
/*    //   For MASTER
	//   32��� (16bit)
    //������������� PLL = 7,168. ����� ������� ������� CODEC_CLK = MCLK*PLL = 12��� * 7,168 = 86.016.000  For MASTER
    AIC3204_rset( 5,  0x91 );  // PLL setting: Power up PLL, P=1 and R=1
    AIC3204_rset( 6,  0x07 );  // PLL setting: J=7
    AIC3204_rset( 7,  0x06 );  // PLL setting: HI_BYTE(D=1680)
    AIC3204_rset( 8,  0x90 );  // PLL setting: LO_BYTE(D=1680)

    //��������� DOSR, NDAC, MADC ��� ����� FS(32���) ��������� �� CODEC_CLK (FS*DOSR*MDAC*NDAC = CODEC_CLK)  For MASTER
	//CODEC_CLK = MCLK*PLL = 12��� * 7,168 = 86.016.000 = 32��� * 192 * 7 * 2
	//��������� ������ � �������� NDAC � NADC ������ �� ����������� ������� ������ (���. 76)
	AIC3204_rset( 13, 0x00 );  // Hi_Byte(DOSR) for DOSR = 192 decimal or 0x00�0 DAC oversamppling
	AIC3204_rset( 14, 0xC0 );  // Lo_Byte(DOSR) for DOSR = 192 decimal or 0x00�0
    AIC3204_rset( 20, 0x80 );  // AOSR for AOSR = 128 decimal or 0x0080 for decimation filters 1 to 6
    AIC3204_rset( 11, 0x82 );  // Power up NDAC and set NDAC value to 2 (32���)
    AIC3204_rset( 12, 0x87 );  // Power up MDAC and set MDAC value to 7
    AIC3204_rset( 18, 0x87 );  // Power up NADC and set NADC value to 7
    AIC3204_rset( 19, 0x82 );  // Power up MADC and set MADC value to 2 (32���)

    //   24��� (16bit)
    //CODEC_CLK = MCLK*PLL = 12��� * 7,168 = 86.016.000 = 24��� * 128 * 7 * 4
    AIC3204_rset( 13, 0x00 );  // Hi_Byte(DOSR) for DOSR = 128 decimal or 0x00�0 DAC oversamppling
    AIC3204_rset( 14, 0x80 );  // Lo_Byte(DOSR) for DOSR = 128 decimal or 0x00�0
    AIC3204_rset( 20, 0x80 );  // AOSR for AOSR = 128 decimal or 0x0080 for decimation filters 1 to 6
    AIC3204_rset( 11, 0x84 );  // Power up NDAC and set NDAC value to 4 (24���,16bit)
    AIC3204_rset( 12, 0x87 );  // Power up MDAC and set MDAC value to 7
    AIC3204_rset( 18, 0x87 );  // Power up NADC and set NADC value to 7
    AIC3204_rset( 19, 0x84 );  // Power up MADC and set MADC value to 4 (24���,16bit)
*/
    //   22��� (16bit)
    //������������� PLL = 7,168. ����� ������� ������� CODEC_CLK = MCLK*PLL = 12��� * 7,168 = 86.016.000  For MASTER
    AIC3204_rset( 5,  0x91 );  // PLL setting: Power up PLL, P=1 and R=1
    AIC3204_rset( 6,  0x07 );  // PLL setting: J=7
    AIC3204_rset( 7,  0x02 );  // PLL setting: HI_BYTE(D=0560)
    AIC3204_rset( 8,  0x30 );  // PLL setting: LO_BYTE(D=0560)
    //CODEC_CLK = MCLK*PLL = 12��� * 7,056 = 86.016.000 = 22,05��� * 192 * 5 * 4
    AIC3204_rset( 13, 0x00 );  // Hi_Byte(DOSR) for DOSR = 192 decimal or 0x00�0 DAC oversamppling
    AIC3204_rset( 14, 0xC0 );  // Lo_Byte(DOSR) for DOSR = 192 decimal or 0x00�0
    AIC3204_rset( 20, 0x80 );  // AOSR for AOSR = 128 decimal or 0x0080 for decimation filters 1 to 6
    AIC3204_rset( 11, 0x84 );  // Power up NDAC and set NDAC value to 4 (24���,16bit)
    AIC3204_rset( 12, 0x85 );  // Power up MDAC and set MDAC value to 7
    AIC3204_rset( 18, 0x85 );  // Power up NADC and set NADC value to 7
    AIC3204_rset( 19, 0x84 );  // Power up MADC and set MADC value to 4 (24���,16bit)



    //   For SLAVE
    //   32��� (16bit)
	//���������� DOSR, NDAC, MADC ��� ����� FS(32���) ��������� �� CODEC_CLK (FS*DOSR*MDAC*NDAC = CODEC_CLK)
	//CODEC_CLK = BCLK*PLL = (32���*32) * (48,0 * 2) = 98.304.000 = 32��� * 128 * 8 * 3
	//��������� ������ � �������� NDAC � NADC ������ �� ����������� ������� ������ (���. 76)	
/*	AIC3204_rset( 13, 0x00 );  // Hi_Byte(DOSR) for DOSR = 128 decimal or 0x0080 DAC oversamppling
	AIC3204_rset( 14, 0x80 );  // Lo_Byte(DOSR) for DOSR = 128 decimal or 0x0080
    AIC3204_rset( 20, 0x80 );  // AOSR for AOSR = 128 decimal or 0x0080 for decimation filters 1 to 6
    AIC3204_rset( 11, 0x83 );  // Power up NDAC and set NDAC value to 3
    AIC3204_rset( 12, 0x88 );  // Power up MDAC and set MDAC value to 8
    AIC3204_rset( 18, 0x88 );  // Power up NADC and set NADC value to 8
    AIC3204_rset( 19, 0x83 );  // Power up MADC and set MADC value to 3
*/

    // DAC ROUTING and Power Up
    AIC3204_rset( 0,  0x01 );  // Select page 1
    AIC3204_rset( 12, 0x08 );  // LDAC AFIR routed to HPL
    AIC3204_rset( 13, 0x08 );  // RDAC AFIR routed to HPR
    AIC3204_rset( 0,  0x00 );  // Select page 0
    AIC3204_rset( 64, 0x02 );  // Left vol=right vol
    AIC3204_rset( 65, 0x00 );  // Left DAC gain to 0dB VOL; Right tracks Left
    AIC3204_rset( 63, 0xd4 );  // Power up left,right data paths and set channel
    AIC3204_rset( 0,  0x01 );  // Select page 1
    AIC3204_rset( 16, 0x00 );  // Unmute HPL , 0dB gain
    AIC3204_rset( 17, 0x00 );  // Unmute HPR , 0dB gain
    AIC3204_rset( 9 , 0x30 );  // Power up HPL,HPR
    Wait(100 );  // Wait

    // ADC ROUTING and Power Up
    AIC3204_rset( 0,  0x01 );   // Select page 1
    AIC3204_rset( 51, 0x48);    // power up MICBIAS with AVDD (0x40)or LDOIN 3.3V (0x78) or 1.2V (0x48)//MM - added micbias

    AIC3204_rset( 52, 0x0C);    //IN3L -> Left Positive, 40k
    AIC3204_rset( 54, 0x0C);    //IN3R -> Left Negative, 40k
    AIC3204_rset( 55, 0xC0);    //IN1R -> Right Positive, 40k
    AIC3204_rset( 57, 0x30);    //IN1L -> Right Negative, 40k

/*
    AIC3204_rset( 52, 0x30 );   // IN2L is routed to Left Positive MICPGA with 40k resistance
    AIC3204_rset( 54, 0x03 );   // CM is routed to Left Negative MICPGA via CM2L with 40k resistance
    AIC3204_rset( 55, 0x30 );   // IN2R is routed to Right Positive MICPGA with 40k resistance
    AIC3204_rset( 57, 0xc0 );   // CM is routed to Right Negative MICPGA via CM1R with 40k resistance
*/
    AIC3204_rset( 59, 48 );     // MIC_PGA_L gaine 24dB
    AIC3204_rset( 60, 48 );     // MIC_PGA_R gaine 24dB

    AIC3204_rset( 0,  0x00 );   // Select page 0
    AIC3204_rset( 81, 0xc0 );   // Powerup Left and Right ADC
    AIC3204_rset( 82, 0x00 );   // Unmute Left and Right ADC

    Wait(100 );
    AIC3204_rset( 0,  0x00 );   // Select page 0

    AIC3204_rset( 87,  82 );   // Left Noise �����
    AIC3204_rset( 95,  82 );   // Right Noise �����
    Wait(100 );  // Wait
}

/////////////////////////////////////////////////////////////////////////
// UART functions
/////////////////////////////////////////////////////////////////////////
void UARTinit()
{
    //CSL_UartIsrAddr    isrAddr;

    mySetup.clkInput = GetSysClk();

    IRQ_disable(UART_EVENT);
    IRQ_clear(UART_EVENT);


    UART_init(&uartObj,CSL_UART_INST_0,UART_INTERRUPT);
    //SYS_setEBSR(CSL_EBSR_FIELD_PPMODE, CSL_EBSR_PPMODE_1);
    hUart = (CSL_UartHandle)(&uartObj);
    UART_setup(hUart,&mySetup);
    // Configure and Register the UART interrupts
    //isrAddr.rbiAddr  = uart_rxIsr;

    IRQ_plug (UART_EVENT, &UART_intrDispatch);
    IRQ_enable(UART_EVENT);

    //UART_setCallback(hUart,&isrAddr);
    UART_eventEnable(hUart, CSL_UART_RECVOR_LINE_STATUS_INTERRUPT);
    UART_eventEnable(hUart, CSL_UART_RECVOR_REG_DATA_INTERRUPT);
    flagUART_RX = 0;
}
//--------------------------------------------------------------
tint cmd_count = 0;
interrupt void UART_intrDispatch(void)
{
    Uint16 ev = 0;
    ev = UART_getEventId(hUart);
    if(ev == 2 || ev == 6) // read and timeout
    {
        while(CSL_FEXT(hUart->uartRegs->LSR,UART_LSR_DR))
        {
            bufUART[cmd_count] = CSL_FEXT(hUart->uartRegs->RBR,UART_RBR_DATA);
            if(cmd_count == 3){
                UART_parse();
                cmd_count = 0;
            }
            else
                cmd_count++;
        }
    }
    else
        cmd_count = 0;
}
//----------------------------------------------------------------------------------

void UART_parse()
{
    Uint16 cmd = bufUART[1]*256+bufUART[0];
    switch(cmd)
    {
    case beg_spkr_sel:
        SPKR_SEL = bufUART[3]*256+bufUART[2];
        cmd_name = cmdSPKR_SEL;
        break;
    case beg_mic_sel:
        MIC_SEL = bufUART[3]*256+bufUART[2];
        cmd_name = cmdMIC_SEL;
        break;
    case beg_mic_short:
        MIC_SHORT = bufUART[3]*256+bufUART[2];
        cmd_name = cmdMIC_SHORT;
        break;
    case beg_aer_off_music:
        AER_OFF_MUSIC = bufUART[3]*256+bufUART[2];
        cmd_name = cmdAER_OFF_MUSIC;
        break;
    }
    flagUART_RX = 1;
}
//----------------------------------------------------------------------------------

void UART_params_apply()
{
    switch(cmd_name){
    /*case beg_full_pack:
		aer_sim_config_aer_params(&siu_inst, &siuSetup);
        aer_sim_aep_config(&aepSimInst, &siuSetup.aep_params,
			siuSetup.aep_gain_adj_exp, siuSetup.aep_gain_adj_mant);
        break;*/
    case cmdEMPTY:
        break;
    case cmdSPKR_SEL:
        spkr_sel = SPKR_SEL;
        break;
	case cmdMIC_SEL:
		mic_sel = MIC_SEL;
        switch(MIC_SEL){
            case 0:
                siuSetup.aer_ctl_bitfield_1 = 471;
                        //siuSetup.aer_ctl_bitfield_1 | aer_CTL1_MUTE_ON;
                break;
            case 1:
                siuSetup.aer_ctl_bitfield_1 = 455;
                        //siuSetup.aer_ctl_bitfield_1 & (~aer_CTL1_MUTE_ON);
                break;
            case 2:
                siuSetup.aer_ctl_bitfield_1 = 455;
                        //siuSetup.aer_ctl_bitfield_1 & !aer_CTL1_MUTE_ON;
            case 3:
                siuSetup.aer_ctl_bitfield_1 = 455;
                        //siuSetup.aer_ctl_bitfield_1 & !aer_CTL1_MUTE_ON;

            break;
		}
		aer_sim_config_aer_params(&siu_inst, &siuSetup);
        aer_sim_aep_config(&aepSimInst, &siuSetup.aep_params,
				siuSetup.aep_gain_adj_exp, siuSetup.aep_gain_adj_mant);
		break;
        case cmdMIC_SHORT:
            flagUART_RX = 0;
            AIC3204_rset( 0,  0x00 );   // Select page 0
            if(MIC_SHORT)
            {
                AIC3204_rset( 87,  82 );   // Left Noise ����� -30dB
                AIC3204_rset( 95,  82 );   // Right Noise ����� -30dB
            }
            else
            {
                AIC3204_rset( 87,  0 );   // Left Noise ����� OFF
                AIC3204_rset( 95,  0 );   // Right Noise ����� OFF
            }
            break;
        case cmdAER_OFF_MUSIC:
            aer_off_music = AER_OFF_MUSIC;
            /*AIC3204_rset( 0,  0x00 );   // Select page 0
            if(aer_off_music == 1){
                AIC3204_rset( 14, 0xC0 );
                AIC3204_rset( 11, 0x82 );
            }
            else{
                AIC3204_rset( 14, 0x80 );
                AIC3204_rset( 11, 0x84 );
            }*/
            Wait(200);
            break;
	}		
}

- it does not work.

  • Hi,
    I did so as written in the recommendation. I'm running my project on the development kit of the EHDS. In debug mode, everything is ok. When loading from the SIP flush, the system starts in 1 of 3 or 4 cases.
    Next, the device initialization code:

    void DeviceInit()
    {
    PLL_Obj pllObj;
    PLL_Config *configInfo;
    PLL_Handle hPll;
    Uint32 pllInstId;
    int i;
    Uint16 prcr;

    CSL_SYSCTRL_REGS->PCGCR1 = 0x0000;
    CSL_SYSCTRL_REGS->PCGCR2 = 0x0000;

    IRQ_init(&dispatchTable, 0);
    IRQ_globalDisable();
    IRQ_disableAll();
    IRQ_clearAll();

    IRQ_setVecs((Uint32)&VECSTART);

    // Set PLL
    const PLL_Config pllCfg_100MHz = {0x8C31, 0x0173, 0x0806, 0x0000}; //from 12MHz
    pllInstId = 0;
    PLL_init(&pllObj,pllInstId);
    hPll = &pllObj;
    PLL_reset(hPll);
    configInfo = (PLL_Config *)&pllCfg_100MHz;
    PLL_config(hPll, configInfo);
    Wait(300);
    PLL_enable(hPll);
    Wait(300);

    //Set PinMap
    CSL_FINST(CSL_SYSCTRL_REGS->EBSR, SYS_EBSR_PPMODE, MODE1);
    CSL_FINST(CSL_SYSCTRL_REGS->EBSR, SYS_EBSR_SP1MODE, MODE0);
    CSL_FINST(CSL_SYSCTRL_REGS->EBSR, SYS_EBSR_SP0MODE, MODE1);

    // Enable HWA, CPU, DPORT, MPORT, XPORT, and IPORT in ICR */
    *(volatile ioport Uint16 *)(0x0001) = 0x000E;
    /* Execute idle instruction */
    asm(" idle");

    //Enable peripherals
    CSL_SYSCTRL_REGS->PCGCR1 = 0x1c02;
    CSL_SYSCTRL_REGS->PCGCR2 = 0x0003;

    // Reset all peripherals
    CSL_SYSCTRL_REGS->PSRCR = 0x0020;
    CSL_SYSCTRL_REGS->PRCR = 0x00BB;
    do
    {
    prcr = CSL_SYSCTRL_REGS->PRCR;
    } while (prcr != 0);
    }
  • Hi Aleksander, 

    The initialization looks good at first glance.

    How are you creating the bootimg.bin file? What are your hex55 parameters?

    Can you test your initialization by executing it without having run the GEL file first. Remove the GEL file from the target configuration

    In the target configuration, click on the Advanced tab at the bottom, Click on C55xx then in the field labeled initialization script, delete the path to the GEL file and save.

    Also with this target connection with the GEL removed, you can connect to the target after running your bootloader and check the Program Counter to see where it is. You can determine if the program is executing from ROM or RAM by checking for a high address like 0x00fe0860 through 0x00ffff00. We can use that address to determine exactly where in the bootloader the program is stuck.

    Or if its executing from RAM, you can use your .map file to determine where it is getting stuck.

    If the target cannot connect at all, then it might be an issue with PLL initialization or code execution going to an unexpected address.

    I recommend you take the PLL init from the latest CSL.

    Let us know what you find.

    Hope this helps,
    Mark

  • Hi, Mark.

    Thanks for the help.
    I found a problem. Problem in the initialization of PLL.
    Instead of the code: .

    // Set PLL
    const PLL_Config pllCfg_100MHz = {0x8C31, 0x0173, 0x0806, 0x0000}; //from 12MHz
    pllInstId = 0;
    PLL_init(&pllObj,pllInstId);
    hPll = &pllObj;
    PLL_reset(hPll);
    configInfo = (PLL_Config *)&pllCfg_100MHz;
    PLL_config(hPll, configInfo);
    Wait(300);
    PLL_enable(hPll);
    Wait(300);

    I did like this: 

    *(volatile ioport Uint16 *)(0x1C20) = 0x8C31;
    *(volatile ioport Uint16 *)(0x1C21) = 0x0173;
    *(volatile ioport Uint16 *)(0x1C22) = 0x0806;
    *(volatile ioport Uint16 *)(0x1C23) = 0x0000;
    Wait(4000);
    *(volatile ioport Uint16 *)(0x1C1F) = 0x0001;

    I do not understand why this is so?

  • Hi.

    I disconnected the GEL file. Now the C5535 initialization code is:

    void DeviceInit()
    {
    Uint16 prcr;

    IRQ_init(&dispatchTable, 0);
    IRQ_globalDisable();
    IRQ_disableAll();
    IRQ_clearAll();
    IRQ_setVecs((Uint32)&VECSTART);

    // Set PLL
    //PLL = 100MHz (from 12MHz) / RD+4 * M+4
    *(volatile ioport Uint16 *)(0x1C20) = 0x8C31;
    *(volatile ioport Uint16 *)(0x1C21) = 0x0173;
    *(volatile ioport Uint16 *)(0x1C22) = 0x0806;
    *(volatile ioport Uint16 *)(0x1C23) = 0x0000;
    Wait(4000);
    *(volatile ioport Uint16 *)(0x1C1F) = 0x0001;

    //Set PinMap
    CSL_FINST(CSL_SYSCTRL_REGS->EBSR, SYS_EBSR_PPMODE, MODE1);
    CSL_FINST(CSL_SYSCTRL_REGS->EBSR, SYS_EBSR_SP1MODE, MODE0);
    CSL_FINST(CSL_SYSCTRL_REGS->EBSR, SYS_EBSR_SP0MODE, MODE1);

    // Enable HWA, CPU, DPORT, MPORT, XPORT, and IPORT in ICR */
    *(volatile ioport Uint16 *)(0x0001) = 0x000E;
    /* Execute idle instruction */
    asm(" idle");

    //Enable peripherals
    *(volatile ioport Uint16 *)(0x1C02) = 0x0000;  //PCGCR1
    *(volatile ioport Uint16 *)(0x1C03) = 0x0003;  //PCGCR2

    // Reset all peripherals
    *(volatile ioport Uint16 *)(0x1C04) = 0x0020;   //PSRCR
    *(volatile ioport Uint16 *)(0x1C05) = 0x00FF;  //PRCR
    do
    {
    prcr = *(volatile ioport Uint16 *)(0x1C05); //PRCR;
    } while (prcr != 0);
    }

    Now when working in debug mode everything is OK, as before.

    When downloading from Flash SPI, not all interfaces work. WART does not work. Next, the UART initialization code:

    CSL_UartSetup mySetup = {
    1000,
    19200,
    CSL_UART_WORD8,
    0,
    CSL_UART_DISABLE_PARITY,
    CSL_UART_FIFO_DMA1_DISABLE_TRIG04,
    CSL_UART_NO_LOOPBACK,
    CSL_UART_NO_AFE,
    CSL_UART_NO_RTS
    };

    void UARTinit()
    {
    CSL_Status st;
    mySetup.clkInput = GetSysClk();

    IRQ_disable(UART_EVENT);
    IRQ_clear(UART_EVENT);

    st = UART_init(&uartObj,CSL_UART_INST_0,UART_INTERRUPT);
    if(st != CSL_SOK)
     GPIO_write(hGpio14, CSL_GPIO_PIN14, 1);

    hUart = (CSL_UartHandle)(&uartObj);
    st = UART_setup(hUart,&mySetup);
    if(st != CSL_SOK)
     GPIO_write(hGpio14, CSL_GPIO_PIN14, 1);

    RQ_plug (UART_EVENT, &UART_intrDispatch);

    IRQ_enable(UART_EVENT);

    st = UART_eventEnable(hUart, CSL_UART_RECVOR_LINE_STATUS_INTERRUPT);
    if(st != CSL_SOK)
     GPIO_write(hGpio14, CSL_GPIO_PIN14, 1);
    st = UART_eventEnable(hUart, CSL_UART_RECVOR_REG_DATA_INTERRUPT);
    if(st != CSL_SOK)
     GPIO_write(hGpio14, CSL_GPIO_PIN14, 1);

    flagUART_RX = 0;
    }

    I repeat that in debug mode UART works horoscho. The problem is only when loading from flash.