Part Number: EVMX777G-01-20-00
Tool/software: Linux
Hi.
I'm using TDA2X evm board with PROCESSOR_SDK_VISION_03_03_00_00. I followed the instruction from VisionSDK_Linux_UserGuide to make bootable sd card.
I didn't make any change to SDK.
But, when I try to boot by sdcard, kernel boot stops after "Starting kernel ..."
Below is my boot log.
U-Boot SPL 2016.05-00009-gac1d50f (Jul 06 2018 - 14:53:50)
DRA722-GP ES2.1
no pinctrl for hs200_1_8v
no pinctrl for ddr_1_8v
** First descriptor is NOT a primary desc on 1:1 **
Trying to boot from MMC1
reading dra7-ipu2-fw.lzop
spl_load_file_fat: error reading file dra7-ipu2-fw.lzop, err - -1
spl: error reading image dra7-ipu2-fw.lzop, err - -1
Error loading remotecore IPU2!,Continuing with boot ...
reading dra7-dsp1-fw.lzop
spl_load_file_fat: error reading file dra7-dsp1-fw.lzop, err - -1
spl: error reading image dra7-dsp1-fw.lzop, err - -1
Error loading remotecore DSP1!,Continuing with boot ...
reading dra7-dsp2-fw.lzop
spl_load_file_fat: error reading file dra7-dsp2-fw.lzop, err - -1
spl: error reading image dra7-dsp2-fw.lzop, err - -1
Error loading remotecore DSP2!,Continuing with boot ...
reading dra7-ipu1-fw.lzop
spl_load_file_fat: error reading file dra7-ipu1-fw.lzop, err - -1
spl: error reading image dra7-ipu1-fw.lzop, err - -1
Error loading remotecore IPU1!,Continuing with boot ...
reading u-boot.img
reading u-boot.img
reading u-boot.img
reading u-boot.img
U-Boot 2016.05-00009-gac1d50f (Jul 06 2018 - 14:53:50 +0900)
CPU : DRA722-GP ES2.1
Model: TI DRA71 EVM
Board: DRA71x EVM REV A.4
DRAM: 2 GiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
** First descriptor is NOT a primary desc on 1:1 **
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid GPT ***
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid Backup GPT ***
ERROR: cannot find partition: 'userdata'
at arch/arm/cpu/armv7/omap-common/utils.c:199/mmc_get_part_size()
Warning: fastboot.userdata_size: unable to calc
SCSI: SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
Net: Could not get PHY for ethernet@48484000: addr 2
eth0: ethernet@48484000
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading boot.scr
** Unable to read file boot.scr **
reading uEnv.txt
165 bytes read in 2 ms (80.1 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc0 ...
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
3553512 bytes read in 114 ms (29.7 MiB/s)
106677 bytes read in 25 ms (4.1 MiB/s)
Booting from mmc0 ...
Kernel image @ 0x82000000 [ 0x000000 - 0x3638e8 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8ffe2000, end 8ffff0b4 ... OK
Starting kernel ...
---- no response ----
I think kernel image / dtb file are loaded succesfully, but I don't know why kernel boot hangs.
Plz help.
Thanx in advance.