Other Parts Discussed in Thread: OMAP3530
We want to use the OMAP3530 Host USB controlled by the DSP (IVA2.2).
We can get the USB to work if we start Linux & use that to load the DSP.
However, if we attempt to run the DSP in "Standalone Mode" using the Emulator, the Host USB doesn't work.
We can program the USB Host Registers, but don't seem to be getting any data transfers between the USB Module & the DDR2 Memory.
What are the steps required to get the Host USB fully operational on the OMAP3530?
So far
- we have disabled the DSP's cache (had some DSP cache vs. Memory issues)
- we are enabling the clocks in the PRCM (CM_FCLKEN_USBHOST, CM_ICLKEN_USBHOST, CM_ICLKEN3_CORE, CM_FCLKEN3_CORE)
- I thought it might be an L3 Firewall Issue, but checking the various register configurations, it looks like we're using the default values for both Linux & Stand Alone
The Registers I've explicitly checked are:
- L3 Initiator Agent (USB Host), L3 Target Agent (SMS), L3 Protection Mechanism (5.2.5.4), SMS Register Manual (11.2.7). They all seem to be default for both Linux & Stand Alone.
Any thoughts on what's missing.
Please advise.