Part Number: TMDSICE3359
Tool/software: TI-RTOS
Hi,
I am trying to follow the Processor SDK Boot Guide here
.
I am unable to make the bootloader file. I get an error that gmake is not a valid comment. It doesn't happen while setting up the SDK.
Secondly, there is no clear instruction of where to run the make command. That detail is completely missing. It would be helpful is someone helps clear that.
Thirdly, I have tried flashing the bootloader and the application image into the sd card and also to mcspi. The code I tried was the EtherCAT slave demo. But I don't get any response from the board in the case of mcspi.
In the case of the SD card, the UART Terminal just shows that the application is executing. There is no response from the board. By response I refer to the LCD Screen activation and LED blinking on the ICE board in case of directly debugging it through CCS.
Any guidance on this would be very very beneficial.
This would help accelerate our development in the right direction.
Regards,
Keyshav