Part Number: AM3351
Tool/software: Linux
Hi,
Please share the detailed steps to craete squashfs for beagle bone black and boot settings to mount squashfs using u-boot.
Thanks,
Mrudula
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM3351
Tool/software: Linux
Hi,
Please share the detailed steps to craete squashfs for beagle bone black and boot settings to mount squashfs using u-boot.
Thanks,
Mrudula
Hi,
I have downloaded ti-sdk (ti-processor-sdk-linux-am335x-evm-04.03.00.05-Linux-x86-Install.bin). I flashed sd card using create-sdcard.sh script. I could not boot up from sd card. My board is booting from sd card even though boot pin is set sd condition.
Please guide me in building sd card from prebuilt images of ti.
Thanks,
Mrudula
Hi,
I created squash filesystem using mksquash command as mentioned by kemal
sudo tar xvf tisdk-rootfs-image-am335x-evm.tar.xz -C rootfs/
sudo mksquashfs rootfs/ filesystem.squashfs
sudo mkdir -p rootfs/media/ram
and created sd card using create_sdcard.sh script available in bin directory of TI SDK.
Copied filesystem.squashfs using dd command as below
sudo dd if=filesystem.squashfs of=/dev/sdc2
Created uEnv.txt file under boot directory of sd card. boot directory contains prebuilt MLO, u-boot.img from TI SDK.
When tried to boot up with this sd card I get below log:
U-Boot SPL 2017.01-gc68ed086bd (Mar 26 2018 - 15:08:11)
Trying to boot from MMC1
reading uboot.env
** Unable to read "uboot.env" from mmc0:1 **
Using default environment
reading u-boot.img
reading u-boot.img
reading u-boot.img
reading u-boot.img
U-Boot 2017.01-gc68ed086bd (Mar 26 2018 - 15:08:11 -0400)
CPU : AM335X-GP rev 2.1
Model: TI AM335x BeagleBone Black
DRAM: 512 MiB
NAND: 0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
reading uboot.env
** Unable to read "uboot.env" from mmc0:1 **
Using default environment
<ethaddr> not set. Validating first E-fuse MAC
Net: Could not get PHY for cpsw: addr 0
cpsw, usb_ether
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading boot.scr
** Unable to read file boot.scr **
reading uEnv.txt
33 bytes read in 3 ms (10.7 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc0 ...
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:1...
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
Failed to mount ext2 filesystem...
** Unrecognized filesystem type **
SD/MMC found on device 1
** Invalid partition 2 **
## Error: "bootcmd_nand0" not defined
starting USB...
USB0: Port not available.
using musb-hdrc, OUT ep1out IN ep1in STATUS ep2in
MAC a8:1b:6a:1c:3b:a3
HOST MAC de:ad:be:af:00:00
RNDIS ready
ERROR: The remote end did not respond in time.
at /oe/bld/build-CORTEX_1/arago-tmp-external-linaro-toolchain/work/am335x_evm-linux-gnueabi/u-boot-ti-staging/2017.01+gitAUTOINC+c68ed086bd-r21/git/drivers/usb/gadget/ether.c:2426/_usb_eth_init()
missing environment variable: pxeuuid
Retrieving file: pxelinux.cfg/01-a8-1b-6a-1c-3b-a3
using musb-hdrc, OUT ep1out IN ep1in STATUS ep2in
MAC a8:1b:6a:1c:3b:a3
HOST MAC de:ad:be:af:00:00
RNDIS ready
ERROR: The remote
From above log it seems like it could not fine correct partition/ filesystem type and looks like trying to boot from USB.
Could you please help on setting bootargs or mmc_args and how to boot from mmc.
Thanks,
Mrudula
I am still having a problem. When I copied squashed filesystem using dd command to SD card, u-boot is not able to recognize this partition and not able to read uEnv.txt file. I created separate boot partition having MLO, u-boot.img and uEnv.txt file. But with this changes also not able to boot.