Part Number: AM5728
Dear all,
I was trying to install Xorg compatible GPU driver on my Sitara AM5728 IDK. I came to know that there is a GPU driver source file in a folder "ti-sgx-ddk-km-1.14.3699939", which comes with the TI SDK for Sitara AM57xx SoC. I have managed to compile the source and this process produced two kernel modules file "bc_example.ko and pvrsrvkm.ko" as an output. I have loaded these kernel modules, as you may see in the lsmod snapshot below
My questions are as follows:
1) Will TI provided GPU driver sources produce only two kernel modules files as mentioned above or Will it also produce some additional files too? If it produce additional files, then what are those files and how can they be obtained?
2) There is also http://processors.wiki.ti.com/index.php/Graphics_SDK_Quick_installation_and_user_guide#Xorg_build which is a complete Graphic SDK provided by TI. However, it seems that this is not compatible to AM5728 SoC. Could you send me the link of such Graphic SDK for AM5728 IDK?
3) If these two kernel modules are the only driver files needed, then how can I configure Xorg to use this driver?
Look forward to receiving your response.
- Farrukh