I note that the current technical manual lacks a chapter on the PCIe interface - I assume this will be added soon?.
Also, do you have any numbers on the PCIe throughput , as both master and slave read & write.
thanks
steve
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I note that the current technical manual lacks a chapter on the PCIe interface - I assume this will be added soon?.
Also, do you have any numbers on the PCIe throughput , as both master and slave read & write.
thanks
steve
Steve,
An updated version of the TRM will be made available soon that includes additional content, including a chapter on the PCIe interface.
Here are some raw throughput benchmark numbers. In a real application the throughput could be a little less due to SW stack overhead, the response time of the PCIe device on the other side, and application memory bandwidth sharing by the other internal HW components.
|
Data Block Size |
Raw Throughput |
|
1KB |
208MB/s |
|
2KB |
333MB/s |
|
4KB |
456MB/s |
|
8KB |
556MB/s |
|
16KB |
626MB/s |
|
32KB |
673MB/s |
|
64KB+ |
700MB/s |
Low throughput numbers for the smaller data block sizes are due to SW and protocol overhead.
Regards,
Marc Pyne
The reason I ask, is that the DM642 had some PCI throughput issues - see a post called
and I want to make sure TI has resolved these with the PCIe interface.
thanks
steve
Steve,
The source is DDR[0].
I am looking into the PCI Bus Master Throughput issue, but PCIe is very different from PCI from both a hardware and protocol perspective, so I don't expect that there would be the same issue in these devices.
Regards,
Marc
Hi
We are looking for ARM Development Kit which has PCI Express interface
and Android support ?
We found from online search, DM816x has this support:
http://www.windowsfordevices.com/c/a/News/TI-TMS320DM8168-and-TMS320DM8148-DaVinci-chips/
But seems like the platform doesn't have Android support as of now. But
from the above link, it states will be available from 2nd Quarter of
2011.
Is there any existing Android Support ARM EVM kit with PCI Express
Interface ?
Thanks for your information in advance.
Thanks,
Vijaydeep.G
Hello,
Please refer to this link for the AM389x devices:
http://focus.ti.com/docs/toolsw/folders/print/androidsdk-sitara.html
Regards,
Marc