Tool/software: TI-RTOS
Hello,
I modified IssIspSimcop_Display usecase.
I inserted New algo_link between IssCapture and IssM2mIsp link.
But, It looks not good.
I cannot see command menu of usecase link this.
[IPU1-0] Vision SDK Usecases,
[IPU1-0] --------------------
[IPU1-0] 1: Single Camera Usecases
[IPU1-0] 2: Multi-Camera LVDS Usecases
[IPU1-0] 3: AVB RX Usecases, (TDA2x & TDA2Ex ONLY)
[IPU1-0] 4: Dual Display Usecases, (TDA2x EVM ONLY)
[IPU1-0] 5: ISS Usecases, (TDA3x ONLY)
[IPU1-0] 6: TDA2x Stereo Usecases
[IPU1-0] 7: Network RX/TX Usecases
[IPU1-0] a: Miscellaneous test's
[IPU1-0] f: TIDL Usecase
[IPU1-0]
[IPU1-0] s: System Settings
[IPU1-0]
[IPU1-0] x: Exit
[IPU1-0]
[IPU1-0] Enter Choice:
[IPU1-0]
[IPU1-0] 25.469651 s:
[IPU1-0] 25.469773 s:
[IPU1-0]
[IPU1-0] ISS Usecases (TDA3x ONLY)
[IPU1-0] ---------------------------
[IPU1-0] 1: 1CH ISS capture + ISS ISP + ISS LDC+VTNF + Display
[IPU1-0] 2: 4CH ISS capture + ISS ISP + Simcop + Surround View (DSP1) + Display
[IPU1-0] 4: 3D SRV 4CH ISS capture + ISS ISP + DeWarp + Synthesis (DSP1) + Display
[IPU1-0] 5: Surround View Calibration
[IPU1-0] 6: 3D + 2D SRV 4CH ISS capture + ISS ISP + DeWarp + Synthesis (DSP1) + Display
[IPU1-0] c: 4 Channel (2 ch per CSI2 Inst) ISS Capture (OV2775 Sensor) Display
[IPU1-0]
[IPU1-0] x: Exit
[IPU1-0]
[IPU1-0] Enter Choice:
[IPU1-0]
[IPU1-0] 28.020496 s: ISSCAPTURE: Create in progress !!!
[IPU1-0] 28.021899 s: UTILS: DMA: Allocated CH (TCC) = 48 (48)
[IPU1-0] 28.022021 s: UTILS: DMA: 0 of 1: Allocated PaRAM = 48 (0x63304800)
[IPU1-0] 28.022265 s: ISSCAPTURE: Create Done !!!
[IPU1-0] 28.022631 s: ALGORITHM: Create in progress (algId = 14) !!!
[IPU1-0] 28.216677 s: ALGORITHM: Create Done (algId = 14) !!!
[IPU1-0] 28.216830 s: ISSM2MISP: Create in progress !!!
[IPU1-0] 28.217806 s: UTILS: DMA: Allocated CH (TCC) = 49 (49)
[IPU1-0] 28.217928 s: UTILS: DMA: 0 of 1: Allocated PaRAM = 49 (0x63304820)
[IPU1-0] 28.222137 s: ISSM2MISP: Memory requirement is 13231488 bytes.
[IPU1-0] 28.222229 s: ISSM2MISP: Memory provided by user is 15305088 bytes.
[IPU1-0] 28.222320 s: ISSM2MISP: Unused Memory is 2073600 bytes.
[IPU1-0] 28.222442 s: ISSM2MISP: Create Done !!!
[IPU1-0] 28.222595 s: ALGORITHM: Create in progress (algId = 6) !!!
[IPU1-0] 28.223113 s: ALGORITHM: Create Done (algId = 6) !!!
[IPU1-0] 28.223632 s: ISS Resizer: Create in progress !!!
[IPU1-0] 28.227627 s: ISS RESIZER: Create Done !!!
[IPU1-0] 28.227780 s: DISPLAY: Create in progress !!!
[IPU1-0] 28.228329 s: DISPLAY: Create Done !!!
[IPU1-0] 28.228512 s: ALGORITHM: Create in progress (algId = 3) !!!
[IPU1-0] 28.246202 s: ALG_ISS_AEWB: Memory requirement is 870396 bytes.
[IPU1-0] 28.246324 s: ALG_ISS_AEWB: Memory provided by user is 917504 bytes.
[IPU1-0] 28.246629 s: ALG_ISS_AEWB: Unused Memory is 47108 bytes.
[IPU1-0] 28.246721 s: ALGORITHM: Create Done (algId = 3) !!!
[IPU1-0] 28.246873 s: ISSM2MSIMCOP: Create in progress !!!
[IPU1-0] 28.247788 s: UTILS: DMA: Allocated CH (TCC) = 50 (50)
[IPU1-0] 28.247910 s: UTILS: DMA: 0 of 1: Allocated PaRAM = 50 (0x63304840)
[IPU1-0] 28.249435 s: ISSM2MSIMCOP: Create Done !!!
[IPU1-0] 28.249618 s: DISPLAY: Create in progress !!!
[IPU1-0] 28.250137 s: DISPLAY: Create Done !!!
[IPU1-0] 28.250533 s: GRPXSRC: Create in progress !!!
[IPU1-0] 29.768315 s: GRPXSRC: Create Done !!!
[IPU1-0] 29.768803 s: DISPLAY: Create in progress !!!
[IPU1-0] 29.769291 s: DISPLAY: Create Done !!!
[IPU1-0] 29.769871 s: SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1022
[IPU1-0] 29.769993 s: SYSTEM: Heap = LOCAL_DDR @ 0x00000000, Total size = 262144 B (256 KB), Free size = 235976 B (230 KB)
[IPU1-0] 29.770145 s: SYSTEM: Heap = SR_OCMC @ 0x00000000, Total size = 0 B (0 KB), Free size = 0 B (0 KB)
[IPU1-0] 29.770359 s: SYSTEM: Heap = SR_DDR_CACHED @ 0x88103000, Total size = 368037888 B (350 MB), Free size = 301700608 B (287 MB)
[IPU1-0] 29.770542 s: SYSTEM: Heap = SR_DDR_NON_CACHED @ 0xbfc00000, Total size = 129792 B (0 MB), Free size = 129792 B (0 MB)
[IPU1-0] 29.771030 s: QSPI Read Started, please wait!
[IPU1-0] 29.771213 s: QSPI Read Completed Sucessfully
[IPU1-0] 29.773317 s: CHAINS: DCC Tag ID check failed for QSPI
[IPU1-0] 29.773409 s: CHAINS: Using DCC Profile from Driver
[IPU1-0] 29.781766 s: *** UTILS: CPU KHz = 20000 Khz ***
[IPU1-0] 32.069541 s: Setting Camera Power to 3!!!
[IPU1-0] 32.069633 s: Waiting for 2000 milliseconds!!!
[IPU1-0] 34.069602 s: Serilaizer # 0 has I2CAddr 74 !!!
[IPU1-0] 68.152626 s: ### Enablig CSI output
[IPU1-0] 68.552949 s: #### Sensor Config time = 38770 msec ####
[IPU1-0] 68.553284 s: DISPLAY: Start in progress !!!
[IPU1-0] 68.553345 s: DISPLAY: Start Done !!!
[IPU1-0] 68.562923 s: DISPLAY: Start in progress !!!
A usecase hang-on in this stauts, and any output/input are not processed.
Could you give me some advice why this situation accured?
Thank you.