This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

optimize option

In my project have several files,and have a DSP/BIOS Config .

     when I specify the   -o3 option,then build ,then run. Due to the complicated optimzing  procedure ,i  met errors.So, I want to complile the files separately with differently optimzing options.But i am not familiar with that.

   So if someone can tell me  how to compile different file with different optimzing options?  If that can be done in build option   item?

  It is  better if a project example  can be provied.

 

 

  • Which DSP are you using?

    Which version of CCS are you using?

    Which version of Code Generation Tools are you using?

    In CCSv3, I believe the procedure is to right-click on a source file in the Project window and select File-Specific Options, or something like that.

    In CCSv4, it is similar but you right-clock on the filename and select Build Options, if my memory is correct.

    If these do not help you, we can move this thread to the Code Composer Studio forum.

     

    If this answers your question, please click the  Verify Answer  button below. If not, please reply back with more information.