Hi,
I have a custom board that I am trying to flash using UART1. I can see the BOOTME coming over the serial line but the flasher tool gives me the "Waiting for SFT on the OMAP-L138..." message.
I guess that the problem is that the ubl is communicating on UART2 instead of UART1. How can I fix that? I have the environment setup for recompiling the flasher tools and ubl files.
Is it also possible to use the u-boot directly without flashing the ubl file? I guess I need to setup the information needed for mDDR and SPI, right?
Best Regards,
Niclas