Hi E2E Team,
When powering on the TDA2Px EVM I’m not getting any UART console message or output on the HDMI monitor, however I do see 2 solid green lights that are labeled “Console” and “12V”, as well as a spinning fan.
The contents of my FAT32 formatted SD card are below(files provided by an apps engineer):
The dip-switch settings are set for SD card boot mode, see below,
and the top of the board is connected as seen below(I've since plugged in the 12V power cord to the sensor fusion board, but don't think it was causing the initial problem).
And when connecting to the console I’m using the below settings:
Please let me know your thoughts as to why I’m not able to communicate with the device.
Thanks,
Barend