Other Parts Discussed in Thread: OMAP3530
Hi everybody,
I have some problem with loop sample. I'm using OMAP3530 EVM board.
I changed some configuration in loop sample.
I increased poolSize, DDR2.heapSize, so that I can run loop sample with the size of buffer up to 65536, but it still has some problem.
It just runs successfully with 1 iteration, and it went failed when the number of iteration is more than 1.
When iteration = 2, output is listed below:
=============== Sample Application : LOOP ==========
==== Executing sample for DSP processor Id 0 ====
SMAPOOL
Entered LOOP_Create ()
Leaving LOOP_Create ()
Entered LOOP_Execute ()
CHNL_issue failed (input). Status = [0x80040709]
Leaving LOOP_Execute ()
Entered LOOP_Delete ()
Leaving LOOP_Delete ()
Can anyone help me to figure it out?
I very thank you!