Hi All,
I have a question on the meaning of “latched by VD”.
This appears frequently in 643x VPFE document, SPRU977a, for example, in page 126, Table 58, both register bit WEN (data write enable) and LPF (low-pass filter) are said to be “latched by VD”.
What is “VD”?
1. First, for digital video signal such as BT.656, there are embedded sync signal within the stream, so VSYNC and HSYNC can be extracted from the stream. Does VD refer to VSYNC? If true, isn’t the “latching” too frequent? Because for BT.656 sampling of NTSC, depending on how one counts, every minute there are at least 60 VSYNC. Why there needs to be so many latching action?
2. Second, or does VD refer to VDINT0, VDINT1 and VDINT2 interrupts on page 32, Table 10 – “DSP Interrupts – VPFE”?
The last question is what is “latching”? I am new to electronics, but it is basic knowledge that D Flip-Flops, which are basic structure of registers, latch new value on the rising edge of the clock signal. So does “latch” refer to this? After all, the contexts where “latched by VD” appear are instructions on register configuration.
Sincerely,
Zheng